Wiki

This version (30 Mar 2015 15:36) was approved by Andrei Cozma.

QDESYS Motor Control IP & EtherCAT Design

QDESYS provides the following reference designs for the AD-FMCMOTCON2-EBZ

  • EtherCAT design showing how to do real time motor control over the network
  • A high performance Field Oriented Controller (FOC). The FOC algorithm is provided as a highly optimized IP that can be integrated in the FPGA project. Below you can find a few screenshots from the user application provided with the IP taken while running with the AD-FMCMOTCON2-EBZ.

Main panel PWM control panel Current settings panel RPFM control panel

Phase currents Stator Currents vs Space

Navigation - AD-FMCMOTCON2-EBZ

resources/eval/user-guides/ad-fmcmotcon2-ebz/qdesys_ip.txt · Last modified: 30 Mar 2015 15:35 by Andrei Cozma