Wiki

This version (21 Jul 2015 09:03) was approved by LucianS.The Previously approved version (27 Apr 2015 14:20) is available.Diff

ADI FMC Motor Drive System v2 Introduction

The ADI FMC motor drive v2 solution consist of the following products

  • AD-FMCMOTCON2-EBZ - Controller board. Compatible with all Xilinx FPGA platforms with FMC LPC or HPC connectors.
  • AD-DRVLV2-EBZ - Low voltage drive board. Connects to the Controller board and has a power stage that can drive Brushed DC / BLDC / PMSM / Stepper motors up to 48V and 20A.
  • AD-DYNO2-EBZ - Dynamometer drive system. Acts as an electronically adjustable load with two BLDC motors connected in a dyno setup.
AD-FMCMOTCON2-EBZ AD-DRVLV2-EBZ AD-DYNO2-EBZ
AD-FMCMOTCON2-EBZ AD-DRVLV2-EBZ AD-DYNO1-EBZ

The Controller and the Drive boards are provided as a kit and cannot be purchased separately. They are both distributed under the AD-FMCMOTCON2-EBZ part number.

Purpose

  • Provide an efficient drive system for different types of electric motors
  • Address power and isolation challenges encountered in motor control applications
  • Provide accurate measurement of motor feedback signals
  • Achieve flexible control with FPGA/SoC interface
  • High speed industrial Ethernet interface

Added Value

  • Complete control solution showing how to integrate hardware for
    • Power
    • Isolation
    • Measurement
    • Control
  • Increased control flexibility due to FPGA interfacing capabilities
  • Increased versatility to be able to control different types of motors
  • Example reference designs showing how to use the control solution with Xilinx FPGAs

Where to Buy

Navigation - EVAL-FMCMOTCON2

resources/eval/user-guides/ad-fmcmotcon2-ebz/introduction.txt · Last modified: 21 Jul 2015 09:00 by LucianS