This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | |||
resources:eval:user-guides:ad-fmcmotcon2-ebz:hardware [27 Apr 2015 14:20] Andrei Cozma |
resources:eval:user-guides:ad-fmcmotcon2-ebz:hardware [21 Jul 2015 12:58] Lucian Sin repetitive word |
||
---|---|---|---|
Line 23: | Line 23: | ||
**[[resources/eval/user-guides/ad-fmcmotcon2-ebz/hardware/lv_board|AD-DRVLV2-EBZ]]** - Low voltage drive board\\ | **[[resources/eval/user-guides/ad-fmcmotcon2-ebz/hardware/lv_board|AD-DRVLV2-EBZ]]** - Low voltage drive board\\ | ||
{{:resources:eval:user-guides:ad-fmcmotcon2-ebz:mc2_lv_single.jpg?300|AD-DRVLV2-EBZ}} | {{:resources:eval:user-guides:ad-fmcmotcon2-ebz:mc2_lv_single.jpg?300|AD-DRVLV2-EBZ}} | ||
- | * Connects to the Controller board and has a power stage that can drive drive motors up to 48V and 20A. | + | * Connects to the Controller board and has a power stage that can drive motors up to 48V and 20A. |
* Drives 2 motors simultaneously | * Drives 2 motors simultaneously | ||
* High frequency drive stage implemented with ADI isolated gate drivers | * High frequency drive stage implemented with ADI isolated gate drivers |