This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:ad-fmcmotcon1-ebz [06 May 2014 10:07] – Added top level summary Andrei Cozma | resources:eval:user-guides:ad-fmcmotcon1-ebz [10 Feb 2021 04:46] (current) – add retired Robin Getz | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== AD-FMCMOTCON1-EBZ User Guide ====== | ====== AD-FMCMOTCON1-EBZ User Guide ====== | ||
+ | {{page>/ | ||
The **[[adi> | The **[[adi> | ||
- | The purpose of the **AD-FMCMOTCON1-EBZ** is to provide a complete motor drive system demonstrating efficient control of multiple motor types. It consists of 2 boards: a controller board and a drive board. The system incorporates high quality power sources; reliable power, control, and feedback signals isolation; accurate measurement of motor current & voltage signals; high speed interfaces for control signals to allow fast controller response; industrial Ethernet high speed interfaces; flexible control with FPGA/SoC interface. | + | The purpose of the **AD-FMCMOTCON1-EBZ** is to provide a complete motor drive system demonstrating efficient control of Brushed DC, BLDC, PMSM and Stepper motors. It consists of 2 boards: a controller board and a drive board. The system incorporates high quality power sources; reliable power, control, and feedback signals isolation; accurate measurement of motor current & voltage signals; high speed interfaces for control signals to allow fast controller response; industrial Ethernet high speed interfaces; flexible control with FPGA/SoC interface. |
The **AD-DYNO1-EBZ** dynamometer is provided as an extension of the drive system. This is a dynamically adjustable load that can be used to test real-time motor control performance. It consists of two BLDC motors directly coupled through a rigid connection. One of the BLDC motors acts as a load and is controlled by the DYNO’s embedded control system while then second motor is driven by the **AD-FMCMOTCON1-EBZ**. | The **AD-DYNO1-EBZ** dynamometer is provided as an extension of the drive system. This is a dynamically adjustable load that can be used to test real-time motor control performance. It consists of two BLDC motors directly coupled through a rigid connection. One of the BLDC motors acts as a load and is controlled by the DYNO’s embedded control system while then second motor is driven by the **AD-FMCMOTCON1-EBZ**. | ||
Line 29: | Line 30: | ||
- [[.: | - [[.: | ||
- [[.: | - [[.: | ||
- | - [[.: | ||
- [[.: | - [[.: | ||
- [[.: | - [[.: | ||
- [[.: | - [[.: | ||
+ | |||
+ | ====== Videos ====== | ||
+ | |||
+ | ADI/ | ||
+ | |||
+ | {{analogTV> | ||
+ | |||
+ | |||
+ | From ADI's 2013 Design Conference | ||
+ | {{youtube> |