Wiki

This version (10 Feb 2021 04:41) was approved by Robin Getz.The Previously approved version (12 Sep 2014 13:13) is available.Diff

Hardware Setup Guide

Analog Devices uses six designations to inform our customers where a semiconductor product is in its life cycle. From emerging innovations to products which have been in production for twenty years, we understand that insight into life cycle status is important. Device life cycles are tracked on their individual product pages on analog.com, and should always be consulted before making any design decisions.

This particular articl/edocument/design has been retired or deprecated, which means it is no longer maintained or actively updated, even though the devices themselves may be Recommended for New Designs or in Production. This page is here for historical/reference purposes only.

Supported Carriers

Required Hardware

  • AD-FMCMOTCON1-EBZ - Controller board.
  • AD-DRVLV1-EBZ - Low voltage drive board.
  • AD-DYNO1-EBZ - Dynamo-meter Drive System (Optional).
  • 24V 3A capable lab power supply.

Getting Started

  • Connect the Low voltage drive board to the Controller board.
  • Connect the Controller + Drive boards assembly to FMC connector of the ZedBoard
  • Insert the 6 pin Hall connector into P7 - pin 1 is the empty slot of the Hall connector. In case an encoder is used there is a one to one corespondence of the encoder's pins to the pins of the P7 connector.

Hall connector

  • Insert the 5V supply in the left side of the DYNAMO-METER DRIVE SYSTEM

Dynamo-meter Drive System

  • Ensure that the Emergency Stop button P2 is pressed (more information about drive board buttons here)

Motor and Power connections

  • Insert the 3 pin motor connector into P1 and connect the lab power supply to P4 (more information about drive board connectors here)

Motor and Power connections

  • Power on the ZedBoard
  • After the board is programmed, in order to start the motor, the Emergency Stop button P2 must be released and then the Reset switch S1 must be pressed for a few seconds.

Navigation - AD-FMCMOTCON1-EBZ

resources/eval/user-guides/ad-fmcmotcon1-ebz/quickstart/lv_setup_guide.txt · Last modified: 10 Feb 2021 04:40 by Robin Getz