This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision | ||
resources:eval:user-guides:ad-fmcmotcon1-ebz:quickstart:lv_setup_guide [21 Feb 2014 14:53] – add the last step(release P2, then press S1) for starting the motor Lucian Sin | resources:eval:user-guides:ad-fmcmotcon1-ebz:quickstart:lv_setup_guide [12 Sep 2014 13:13] – [Getting Started] Andrei Cozma | ||
---|---|---|---|
Line 24: | Line 24: | ||
* Connect the Low voltage drive board to the Controller board. | * Connect the Low voltage drive board to the Controller board. | ||
* Connect the Controller + Drive boards assembly to FMC connector of the ZedBoard | * Connect the Controller + Drive boards assembly to FMC connector of the ZedBoard | ||
- | * Insert the 6 pin Hall connector into P7 - pin 1 is the empty slot of the Hall connector | + | * Insert the 6 pin Hall connector into P7 - pin 1 is the empty slot of the Hall connector. In case an encoder is used there is a one to one corespondence of the encoder' |
{{ : | {{ : | ||
* Insert the 5V supply in the left side of the DYNAMO-METER DRIVE SYSTEM | * Insert the 5V supply in the left side of the DYNAMO-METER DRIVE SYSTEM |