Wiki

This version is outdated by a newer approved version.DiffThis version (10 Feb 2014 17:59) was approved by Andrei Cozma.

This is an old revision of the document!


QDESYS Motor Control IP

A FOC implementation targeted for the AD-FMCMOTCON1-EBZ is available from QDESYS. The control algorithm is provided as a highly optimized IP that can be integrated in the FPGA project. Below you can find a few screenshots from the user application provided with the IP taken while running with the AD-FMCMOTCON1-EBZ.

Main panel PWM control panel Current settings panel RPFM control panel

Phase currents Stator Currents vs Space

Navigation - AD-FMCMOTCON1-EBZ

resources/eval/user-guides/ad-fmcmotcon1-ebz/qdesys_ip.1392051585.txt.gz · Last modified: 10 Feb 2014 17:59 by Andrei Cozma