Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:eval:user-guides:ad-fmcmotcon1-ebz:qdesys_ip [10 Feb 2014 17:59]
Andrei Cozma update
resources:eval:user-guides:ad-fmcmotcon1-ebz:qdesys_ip [10 Feb 2021 04:45]
Robin Getz add retired
Line 1: Line 1:
 ====== QDESYS Motor Control IP ====== ====== QDESYS Motor Control IP ======
 +{{page>/​wiki/​common#​retired&​nofooter&​noheader}}
 A FOC implementation targeted for the **AD-FMCMOTCON1-EBZ** is available from **[[http://​www.qdesys.com/​|QDESYS]]**. The control algorithm is provided as a highly optimized IP that can be integrated in the FPGA project. Below you can find a few screenshots from the user application provided with the IP taken while running with the **AD-FMCMOTCON1-EBZ**. A FOC implementation targeted for the **AD-FMCMOTCON1-EBZ** is available from **[[http://​www.qdesys.com/​|QDESYS]]**. The control algorithm is provided as a highly optimized IP that can be integrated in the FPGA project. Below you can find a few screenshots from the user application provided with the IP taken while running with the **AD-FMCMOTCON1-EBZ**.
  
resources/eval/user-guides/ad-fmcmotcon1-ebz/qdesys_ip.txt · Last modified: 10 Feb 2021 04:45 by Robin Getz