This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:ad-fmcmotcon1-ebz:matlab_models [12 Sep 2014 13:34] – [Field Oriented Controller (FOC)] Andrei Cozma | resources:eval:user-guides:ad-fmcmotcon1-ebz:matlab_models [10 Feb 2021 04:45] (current) – add retired Robin Getz | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== Simulink Controller Models ====== | ====== Simulink Controller Models ====== | ||
+ | {{page>/ | ||
The Vivado HDL design is provided with an integrated FOC and speed & torque controller generated from a Simulink model provided by MathWorks. The controller is designed in Simulink and the corresponding HDL code is generated using the Mathworks HDL Coder. | The Vivado HDL design is provided with an integrated FOC and speed & torque controller generated from a Simulink model provided by MathWorks. The controller is designed in Simulink and the corresponding HDL code is generated using the Mathworks HDL Coder. | ||
Line 59: | Line 59: | ||
<WRAP round help 80%> | <WRAP round help 80%> | ||
- | * Questions? [[http://ez.analog.com/ | + | * Questions? [[ez> |
</ | </ | ||
{{navigation AD-FMCMOTCON1-EBZ# | {{navigation AD-FMCMOTCON1-EBZ# |