Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:user-guides:ad-fmcmotcon1-ebz:introduction [10 Feb 2014 22:14] – [Where to Buy] Andrei Cozma | resources:eval:user-guides:ad-fmcmotcon1-ebz:introduction [10 Feb 2021 04:39] (current) – add retired Robin Getz |
---|
====== ADI FMC Motor Control Introduction ====== | ====== ADI FMC Motor Drive System Introduction ====== |
| {{page>/wiki/common#retired&nofooter&noheader}} |
| |
**The ADI FMC motor control solution consist of the following products** | **The ADI FMC motor drive solution solution consist of the following products** |
* **[[resources/eval/user-guides/ad-fmcmotcon1-ebz/hardware/controller_board|AD-FMCMOTCON1-EBZ]]** - Controller board. Compatible with all Xilinx FPGA platforms with FMC LPC or HPC connectors. | * **[[resources/eval/user-guides/ad-fmcmotcon1-ebz/hardware/controller_board|AD-FMCMOTCON1-EBZ]]** - Controller board. Compatible with all Xilinx FPGA platforms with FMC LPC or HPC connectors. |
* **[[resources/eval/user-guides/ad-fmcmotcon1-ebz/hardware/lv_board|AD-DRVLV1-EBZ]]** - Low voltage drive board. Connects to the Controller board and has a power stage that can drive drive Brushed DC / BLDC / PMSM / Stepper motors up to 48V and 18A. | * **[[resources/eval/user-guides/ad-fmcmotcon1-ebz/hardware/lv_board|AD-DRVLV1-EBZ]]** - Low voltage drive board. Connects to the Controller board and has a power stage that can drive drive Brushed DC / BLDC / PMSM / Stepper motors up to 48V and 18A. |
* **[[resources/eval/user-guides/ad-fmcmotcon1-ebz/hardware/dyno|AD-DYNO1-EBZ]]** - Dynamo-meter drive system. Acts as an electronically adjustable load with two BLDC motors connected in a dyno setup. | * **[[resources/eval/user-guides/ad-fmcmotcon1-ebz/hardware/dyno|AD-DYNO1-EBZ]]** - Dynamometer drive system. Acts as an electronically adjustable load with two BLDC motors connected in a dyno setup. |
| |
|< 100% 33% 33% 34% >| | |< 100% 33% 33% 34% >| |