This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:user-guides:ad-fmcmotcon1-ebz:introduction:dc_control [28 Dec 2013 21:50] – Added navigation pane Andrei Cozma | resources:eval:user-guides:ad-fmcmotcon1-ebz:introduction:dc_control [18 Feb 2014 14:18] (current) – syntax error Lucian Sin | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== Brushed DC Motor Control ====== | ====== Brushed DC Motor Control ====== | ||
- | The Brushed DC motor is the simplest type of motor to control, all tht needs to be done is to vary the supply voltage and the motor' | + | The Brushed DC motor is the simplest type of motor to control, all that needs to be done is to vary the supply voltage and the motor' |
A single transistor and diode can control the speed of a dc motor. | A single transistor and diode can control the speed of a dc motor. |