This is an old revision of the document!
Motor Control Hardware
Hardware solutions
-
Compatible with all Xilinx FPGA platforms with FMC LPC or HPC connectors
2 x Gbit Ethernet PHYs for high speed industrial communication
Hall + Differential Hall + Encoder + Resolver interfaces
Current and voltage measurement using isolated ADCs
Xilinx XADC interface
Fully isolated control and feedback signals
-
Connects to the Controller board and has a power stage that can drive drive Brushed DC / BLDC / PMSM / Stepper motors up to 48V and 18A.
Integrated over current protection
Current measurement using isolated ADCs
Bus voltage, phase currents and total current analog feedback signals
PGAs to maximize the current measurement input range
BEMF zero cross detection for sensorless control of PMSM or BLDC motors
-
Two BLDC motors connected in a dyno setup
Electronically adjustable load – the load value is set using the onboard buttons + LCD
Programmable step and ramp load changes
Measurement and display of load motor phase currents
Measurement and display of load motor speed
External control using Analog Discovery
Where to Buy
Downloads
AD-FMCMOTCON1-EBZ
AD-DRVLV1-EBZ