This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:ad-fmcmotcon1-ebz:hardware:signal_chain [02 Jul 2015 14:03] – [Ia, Ib Measurement Signal Chain] Mihai Bancisor | resources:eval:user-guides:ad-fmcmotcon1-ebz:hardware:signal_chain [10 Feb 2021 04:42] (current) – add retired Robin Getz | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== AD-FMCMOTCON1-EBZ Signal Measurement Chain ====== | ====== AD-FMCMOTCON1-EBZ Signal Measurement Chain ====== | ||
+ | {{page>/ | ||
The motor control system allows the measurement of the Ia(phase A current), Ib(phase B current) and It(total current) as well as the measurement of Vbus using signal chains which involve components from both the controller and low voltage driver boards. | The motor control system allows the measurement of the Ia(phase A current), Ib(phase B current) and It(total current) as well as the measurement of Vbus using signal chains which involve components from both the controller and low voltage driver boards. | ||
Line 13: | Line 13: | ||
* The formula for calculating Ia or Ib is: | * The formula for calculating Ia or Ib is: | ||
<m> I = (counts - 32768)*ADCrange / 2^(ADCbits-1)*RS </m> | <m> I = (counts - 32768)*ADCrange / 2^(ADCbits-1)*RS </m> | ||
- | where <m> delim{lbrace}{matrix{3}{1}{{counts = ADC value } {ADCrange = 320e-3 } {ADCbits = 16 }}}{ } </m> | + | where <m> delim{lbrace}{matrix{4}{1}{{counts = ADC value } {RS = 6e-3} {ADCrange = 320e-3 } {ADCbits = 16 }}}{ } </m> |
**Case 2: The ADC is not placed in the proximity of the shunt resistor** | **Case 2: The ADC is not placed in the proximity of the shunt resistor** | ||
Line 23: | Line 23: | ||
* The formula for calculating Ia or Ib is: | * The formula for calculating Ia or Ib is: | ||
<m> I = (counts-32768) * ADCrange/ | <m> I = (counts-32768) * ADCrange/ | ||
- | where <m> delim{lbrace}{matrix{6}{1}{{counts = ADC value } {ADCrange = 320e-3} {ADCbits = 16} {CTRLgain = 1/ | + | where <m> delim{lbrace}{matrix{7}{1}{{counts = ADC value } {RS = 6e-3} {ADCrange = 320e-3} {ADCbits = 16} {CTRLgain = 1/ |
{{: | {{: |