Wiki

This version is outdated by a newer approved version.DiffThis version (11 Jun 2014 16:38) was approved by Andrei Cozma.The Previously approved version (20 May 2014 16:01) is available.Diff

This is an old revision of the document!


DYNO test procedure

Required hardware

  • ZedBoard with mouse and keyboard
  • SD card with ADI Linux image
  • HDMI monitor
  • AD-FMCMOTCON1-EBZ
  • AD-DYNO1-EBZ

Test Procedure

  • In the Linux IIO scope go to the Motor Control tab and select the following configuration:
    • Delta: ON
    • Direction: Clockwise
    • Sensors: hall
    • Controller type: Manual PWM
    • PWM: 90.96%
  • Set Run to ON

Motor Control Tab

  • Make sure that there are no vibrations in the DYNO system.
  • On the DYNO board open the Measurements menu
  • Check the speed & current displayed under Measurements on the DYNO LCD to see if it reads 5200rpm +/- 150rpm for speed and 0.3A for current

Motor Control Tab

  • Set the load to 100%
  • Check the speed & current displayed under Measurements on the DYNO LCD to see if it reads 3200rpm +/- 150rpm for speed and 3.0A +/- 0.1A for current

Motor Control Tab

resources/eval/user-guides/ad-fmcmotcon1-ebz/hardware/dyno_test.1402497523.txt.gz · Last modified: 11 Jun 2014 16:38 by Andrei Cozma