Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:eval:user-guides:ad-fmcmotcon1-ebz:hardware:dyno_test [11 Jun 2014 16:38] – [Test Procedure] Andrei Cozmaresources:eval:user-guides:ad-fmcmotcon1-ebz:hardware:dyno_test [07 Jul 2014 10:10] (current) – [Test Procedure] Andrei Cozma
Line 24: Line 24:
    
   * On the DYNO board open the //Measurements// menu   * On the DYNO board open the //Measurements// menu
-  * Check the speed & current displayed under //Measurements// on the DYNO LCD to see if it reads 5200rpm +/- 150rpm for speed and 0.3A for current+  * Check the speed & current displayed under //Measurements// on the DYNO LCD to see if it reads 5300rpm +/- 250rpm for speed and 0.3A for current
  
 {{:resources:eval:user-guides:ad-fmcmotcon1-ebz:hardware:s2.png?200|Motor Control Tab}} {{:resources:eval:user-guides:ad-fmcmotcon1-ebz:hardware:s2.png?200|Motor Control Tab}}
  
   * Set the load to 100%   * Set the load to 100%
-  * Check the speed & current displayed under //Measurements// on the DYNO LCD to see if it reads 3200rpm +/- 150rpm for speed and 3.0A +/- 0.1A for current+  * Check the speed & current displayed under //Measurements// on the DYNO LCD to see if it reads 3900rpm +/- 250rpm for speed and 1.5A +/- 0.1A for current
  
 {{:resources:eval:user-guides:ad-fmcmotcon1-ebz:hardware:s3.png?200|Motor Control Tab}} {{:resources:eval:user-guides:ad-fmcmotcon1-ebz:hardware:s3.png?200|Motor Control Tab}}
    
      
resources/eval/user-guides/ad-fmcmotcon1-ebz/hardware/dyno_test.txt · Last modified: 07 Jul 2014 10:10 by Andrei Cozma