This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:ad-fmclidar1-ebz [02 Oct 2019 11:32] – [Example] Andrei Cozma | resources:eval:user-guides:ad-fmclidar1-ebz [20 Dec 2023 11:40] (current) – Add obsolesce notice. Stefan-Robert Raus | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== AD-FMCLIDAR1-EBZ ====== | ====== AD-FMCLIDAR1-EBZ ====== | ||
+ | <note warning> | ||
+ | Support for the ad_fmclidar_ebz is discontinued on all supported carriers: Arria10 SOC, zc706 and zcu102. ad_fmclidar_ebz will not be supported in future releases, last release in which pre-build files can be found is 2021_r1. Check this [[: | ||
+ | </ | ||
===== Introduction ===== | ===== Introduction ===== | ||
- | The [[https:// | + | The [[adi>en/ |
**The full system hardware includes:** | **The full system hardware includes:** | ||
Line 44: | Line 46: | ||
<WRAP round info> | <WRAP round info> | ||
- | For more information and how to buy the system please goto the [[https:// | + | For more information and how to buy the system please goto the [[adi>en/ |
</ | </ | ||
Line 75: | Line 77: | ||
===== Application Development ===== | ===== Application Development ===== | ||
- | {{ : | + | {{ : |
The Lidar Prototyping Platform software framework is common across all hardware variants, developed with industry standard tools and interfaces. The necessary parameters are exposed for customers to develop their own proprietary solutions. Support is provided to cover a broad base of operating systems used across different industry areas. There is a proven ADI JESD framework available to reduce development complexity and time, and guarantees deterministic transfer of data from the APD to the host processing system. | The Lidar Prototyping Platform software framework is common across all hardware variants, developed with industry standard tools and interfaces. The necessary parameters are exposed for customers to develop their own proprietary solutions. Support is provided to cover a broad base of operating systems used across different industry areas. There is a proven ADI JESD framework available to reduce development complexity and time, and guarantees deterministic transfer of data from the APD to the host processing system. | ||
<WRAP round download 60%> | <WRAP round download 60%> | ||
- | [[https:// | + | [[https:// |
</ | </ | ||
Line 88: | Line 90: | ||
<WRAP center round important 100%> | <WRAP center round important 100%> | ||
This device complies with International Standards IEC 60825-1: | This device complies with International Standards IEC 60825-1: | ||
- | </ | ||
+ | {{ : | ||
+ | {{ : | ||
+ | </ | ||
---- | ---- | ||
Line 97: | Line 101: | ||
As an example to prove out the overall system functionality a demo using select optics was chosen to have the capability to detect an object of approximately 1m x 1m in size at 60m range with 50% reflective characteristic. | As an example to prove out the overall system functionality a demo using select optics was chosen to have the capability to detect an object of approximately 1m x 1m in size at 60m range with 50% reflective characteristic. | ||
* For the AFE Board a 1" | * For the AFE Board a 1" | ||
- | * For the laser board a custom Fast Axis Collimator optic was selected to narrow the vertical FoV from 15°(natural dispersion of the laser) down to 1° to help achieve the 60m range. Mounting of these lenses requires a custom lens holder and also active lens alignment fitting during the manufacturing process. This was done at [[https:// | + | * For the laser board a custom Fast Axis Collimator optic was selected to narrow the vertical FoV from 30°(natural dispersion of the laser) down to 1° to help achieve the 60m range. Mounting of these lenses requires a custom lens holder and also active lens alignment fitting during the manufacturing process. This was done at [[https:// |
* The lasers were driven at 50KHz with a pulse width of 20ns | * The lasers were driven at 50KHz with a pulse width of 20ns | ||
+ | |||
+ | <WRAP round info 100%> | ||
+ | **Application note:** {{: | ||
+ | </ | ||
---- | ---- | ||
- | ===== Videos ===== | + | ===== Videos |
{{youtube> | {{youtube> | ||
+ | {{youtube> | ||
+ | {{youtube> | ||
+ | |||
+ | {{https:// | ||
+ | |||
+ | [[ adi> | ||
---- | ---- | ||
+ | |||
+ | |||
===== Help and Support ===== | ===== Help and Support ===== | ||
Line 113: | Line 129: | ||
<WRAP round help 60%> | <WRAP round help 60%> | ||
- | [[https://ez.analog.com/ | + | [[ez>depth-perception-ranging-technologies/ |
</ | </ | ||