This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:eval:user-guides:ad-fmclidar1-ebz:system_evaluation [14 Jan 2021 05:11] – user interwiki links Robin Getz | resources:eval:user-guides:ad-fmclidar1-ebz:system_evaluation [30 Jan 2023 01:08] – Joyce Velasco | ||
---|---|---|---|
Line 20: | Line 20: | ||
<WRAP center round info 100%> | <WRAP center round info 100%> | ||
- | * See [[/resources/tools-software/linux-software/ | + | * See [[:resources:tools-software:linux-software: |
- | * The SD card in the box might not have the latest software release. It is recommended to update the software when using the system for the first time by following [[/resources/tools-software/linux-software/ | + | * The SD card in the box might not have the latest software release. It is recommended to update the software when using the system for the first time by following [[:resources:tools-software:linux-software: |
* To prevent the SD from getting corrupted at system power down it is recommended to run this command to safely power down the system: //sudo shutdown -h now// | * To prevent the SD from getting corrupted at system power down it is recommended to run this command to safely power down the system: //sudo shutdown -h now// | ||
</ | </ |