Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:eval:user-guides:ad-fmcjesdadc1-ebz [17 Jul 2015 15:03]
LucianS [Front End]
resources:eval:user-guides:ad-fmcjesdadc1-ebz [22 Feb 2017 19:06] (current)
larsc Canonical spelling of JESD204B
Line 1: Line 1:
 ====== AD-FMCJESDADC1 FMC Board ====== ====== AD-FMCJESDADC1 FMC Board ======
  
-The [[adi>​AD-FMCJESDADC1-EBZ]] is a high speed data acquisition (4 channels at 245.76 MSPS), in a FMC form factor which supports the JESD204-B ​high speed serial interface. This board is one of the few boards that meet all the FMC specifications in terms of mechanical size, and mounting hole locations. For that information,​ please refer to the FMC specification.+The [[adi>​AD-FMCJESDADC1-EBZ]] is a high speed data acquisition (4 channels at 245.76 MSPS), in a FMC form factor which supports the JESD204B ​high speed serial interface. This board is one of the few boards that meet all the FMC specifications in terms of mechanical size, and mounting hole locations. For that information,​ please refer to the FMC specification.
  
 Although this board does meet the FMC specifications,​ it is not meant as a [[wp>​Commercial_off-the-shelf|commercial off the shelf]] (COTS) board. If you want a commercial, ready to integrate product, please refer to one of the many FMC manufactures,​ like [[http://​www.4dsp.com/​fmc176.php|4DSP]]. Although this board does meet the FMC specifications,​ it is not meant as a [[wp>​Commercial_off-the-shelf|commercial off the shelf]] (COTS) board. If you want a commercial, ready to integrate product, please refer to one of the many FMC manufactures,​ like [[http://​www.4dsp.com/​fmc176.php|4DSP]].
Line 13: Line 13:
  
 The card contains: The card contains:
-  * [[adi>​AD9250]] two 14-bit ADC with sampling speeds of up to 250 MSPS, with a [[adi>​JESD204|JESD-204B]] digital interface.+  * [[adi>​AD9250]] two 14-bit ADC with sampling speeds of up to 250 MSPS, with a [[adi>​JESD204|JESD204B]] digital interface.
   * [[adi>​AD9517-1]],​ a multi-output clock distribution device with subpicosecond jitter performance,​ along with an on-chip PLL and VCO.   * [[adi>​AD9517-1]],​ a multi-output clock distribution device with subpicosecond jitter performance,​ along with an on-chip PLL and VCO.
   * [[adi>​ADP151]] an ultralow noise, low dropout linear regulator that operates from 2.2 V to 5.5 V and provides up to 200 mA of output current.   * [[adi>​ADP151]] an ultralow noise, low dropout linear regulator that operates from 2.2 V to 5.5 V and provides up to 200 mA of output current.
Line 93: Line 93:
  
 ==== HDL / Hardware Questions ==== ==== HDL / Hardware Questions ====
 +
 For questions regarding the AD-FMCJESDADC1-EBZ hardware or the HDL reference design please state them in the [[ez>​community/​fpga|FPGA Reference Designs]] sub-community. If you have questions about the tools, please go ask the tools vendors: For questions regarding the AD-FMCJESDADC1-EBZ hardware or the HDL reference design please state them in the [[ez>​community/​fpga|FPGA Reference Designs]] sub-community. If you have questions about the tools, please go ask the tools vendors:
   * [[http://​forums.xilinx.com/​|Xilinx Forums]]   * [[http://​forums.xilinx.com/​|Xilinx Forums]]
Line 98: Line 99:
  
 ==== Linux Driver or Application Questions ==== ==== Linux Driver or Application Questions ====
 +
 For questions regarding the the ADI Linux distribution (which is based [[https://​www.linaro.org/​|Linaro]] with [[http://​www.xfce.org/​|Xfce]] desktop), the Linux drivers, or the device trees for the AD9250 based platforms, please use the [[ez>​community/​linux-device-drivers/​linux-software-drivers|Linux Software Drivers]] sub-community. For questions regarding the the ADI Linux distribution (which is based [[https://​www.linaro.org/​|Linaro]] with [[http://​www.xfce.org/​|Xfce]] desktop), the Linux drivers, or the device trees for the AD9250 based platforms, please use the [[ez>​community/​linux-device-drivers/​linux-software-drivers|Linux Software Drivers]] sub-community.
  
Line 103: Line 105:
  
 ==== No-OS Questions ==== ==== No-OS Questions ====
 +
 For questions regarding the no-OS drivers for AD9250, please use the [[ez>​community/​linux-device-drivers/​microcontroller-no-os-drivers|Microcontroller and No-OS Driver]] sub-community. For questions regarding the no-OS drivers for AD9250, please use the [[ez>​community/​linux-device-drivers/​microcontroller-no-os-drivers|Microcontroller and No-OS Driver]] sub-community.
  
 ==== General AD9250 Questions ==== ==== General AD9250 Questions ====
 +
 Questions about the AD9250, please use the [[ez>​community/​data_converters/​high-speed_adcs|AD9250]] sub-community. Questions about the AD9250, please use the [[ez>​community/​data_converters/​high-speed_adcs|AD9250]] sub-community.
resources/eval/user-guides/ad-fmcjesdadc1-ebz.txt · Last modified: 22 Feb 2017 19:06 by larsc