This guide provides some quick instructions (still takes awhile to download, and set things up) on how to setup the AD-FMCDAQ3-EBZ on:
The ZC706 is build around a XC7Z045 FFG900 – 2 FPGA, which means the design will be overclocked when configured for 1233MSPS. In a production design a XC7Z045 FFG900 –3 FPGA should be used or the lane rate should be within the supported range for the specific FPGA.
All the products described on this page include ESD (electrostatic discharge) sensitive devices. Electrostatic charges as high as 4000V readily accumulate on the human body or test equipment and can discharge without detection.
Although the boards feature ESD protection circuitry, permanent damage may occur on devices subjected to high-energy electrostatic discharges. Therefore, proper ESD precautions are recommended to avoid performance degradation or loss of functionality. This includes removing static charge on external equipment, cables, or antennas before connecting to the device.
You will need to:
Even thought this is Linux, this is a persistent file systems. Care should be taken not to corrupt the file system -- please shut down things, don't just turn off the power switch. Depending on your monitor, the standard power off could be hiding. You can do this from the terminal as well with
sudo shutdown -h now