This guide provides some quick instructions (still takes awhile to download, and set things up) on how to setup the AD-FMCDAQ3-EBZ on VCU118
You will need to:
All the products described on this page include ESD (electrostatic discharge) sensitive devices. Electrostatic charges as high as 4000V readily accumulate on the human body or test equipment and can discharge without detection.
Although the boards feature ESD protection circuitry, permanent damage may occur on devices subjected to high-energy electrostatic discharges. Therefore, proper ESD precautions are recommended to avoid performance degradation or loss of functionality. This includes removing static charge on external equipment, cables, or antennas before connecting to the device.
There are two ways of loading the design. One is using the XCST command line, and the second method is to run the tcl script which takes care of loading the bit file and the Linux image.
In Windows, you can run the XSCT terminal from start menu → Xilinx Design Tools → Xilinx Software Command Line Tool.
****** Xilinx Software Commandline Tool (XSCT) v2021.1 **** SW Build 1933 on 2021-06-09-14:19:58 ** Copyright 1986-2021 Xilinx, Inc. All Rights Reserved. xsct% connect attempting to launch hw_server ****** Xilinx hw_server v2021.1 **** Build date : Jun 10 2021 at 20:17:23 ** Copyright 1986-2021 Xilinx, Inc. All Rights Reserved INFO: hw_server application started INFO: Use Ctrl-C to exit hw_server application ****** Xilinx hw_server v2021.1 **** Build date : Jun 10 2021 at 20:17:23 ** Copyright 1986-2021 Xilinx, Inc. All Rights Reserved. INFO: hw_server application started INFO: Use Ctrl-C to exit hw_server application INFO: To connect to this hw_server instance use url: TCP:127.0.0.1:3121 tcfchan#0 xsct% fpga -f system_top.bit 100% 29MB 1.7MB/s 00:17 xsct% targets 1 xcvu9p 2 MicroBlaze Debug Module at USER2 3 MicroBlaze #0 (Running) 4 Legacy Debug Hub xsct% target 3 xsct% targets 1 xcvu9p 2 MicroBlaze Debug Module at USER2 3* MicroBlaze #0 (Running) 4 Legacy Debug Hub xsct% dow simpleImage.vcu118_fmcdaq3.strip Downloading Program -- C:/Users/PPop/Downloads/simpleImage.vcu118_fmcdaq3/simpleImage.vcu118_fmcdaq3.strip section, .text: 0x80000000 - 0x804763ab section, __fdt_blob: 0x804763ac - 0x804863ab section, .rodata: 0x80487000 - 0x808b110f section, .builtin_fw: 0x808b1110 - 0x808b1133 section, __ksymtab: 0x808b1134 - 0x808b746b section, __ksymtab_gpl: 0x808b746c - 0x808bc483 section, __ksymtab_strings: 0x808bc484 - 0x808d6973 section, __param: 0x808d6974 - 0x808d6e5f section, __modver: 0x808d6e60 - 0x808d6fff section, __ex_table: 0x808d7000 - 0x808d844f section, .notes: 0x808d8450 - 0x808d848b section, .sdata2: 0x808d848c - 0x808d8fff section, .data: 0x808d9000 - 0x8095893f section, .init.text: 0x80959000 - 0x8097a75b section, .init.data: 0x8097a75c - 0x8097c053 section, .init.ivt: 0x8097c054 - 0x8097c07b section, .init.setup: 0x8097c07c - 0x8097c3f3 section, .initcall.init: 0x8097c3f4 - 0x8097c80f section, .con_initcall.init: 0x8097c810 - 0x8097c813 section, .init.ramfs: 0x8097c814 - 0x80c2a9fb section, .bss: 0x80c2b000 - 0x80c4225b 100% 12MB 0.2MB/s 00:56 Setting PC to Program Start Address 0x80000000 Successfully downloaded C:/Users/PPop/Downloads/simpleImage.vcu118_fmcdaq3/simpleImage.vcu118_fmcdaq3.strip xsct% Info: MicroBlaze #0 (target 3) Stopped at 0x0 (Stop) xsct% con Info: MicroBlaze #0 (target 3) Running xsct% disconnect xsct% Info: tcfchan#0 closed
Run Vivado TCL Shell from Windows start menu → Xilinx Design Suite → Vivado → Vivado TCL Shell. (In Linux, source the settings.sh file first)
****** Vivado v2021.1 (64-bit) **** SW Build 3247384 on Thu Jun 10 19:36:33 MDT 2021 **** IP Build 3246043 on Fri Jun 11 00:30:35 MDT 2021 ** Copyright 1986-2021 Xilinx, Inc. All Rights Reserved. Vivado% cd \path\to\simpleImage.vcu118_fmcdaq3 Vivado% xsct run.tcl ***** Xilinx hw_server v2021.1 **** Build date : Jun 10 2021 at 20:17:23 ** Copyright 1986-2021 Xilinx, Inc. All Rights Reserved. INFO: hw_server application started NFO: To connect to this hw_server instance use url: TCP:127.0.0.1:3121 Vivado%
user | password |
---|---|
root | analog |
Ramdisk addr 0x00000000, Compiled-in FDT at 0x804763ac Linux version 4.19.0-g17f4223 (jenkins@romlxbuild1.adlk.analog.com) (gcc version 8.2.0 (crosstool-NG 1.20.0)) #1866 Tue Jul 27 13:47:17 IST 2021 setup_memory: max_mapnr: 0x30000 setup_memory: min_low_pfn: 0x80000 setup_memory: max_low_pfn: 0xb0000 setup_memory: max_pfn: 0xb0000 Zone ranges: DMA [mem 0x0000000080000000-0x00000000afffffff] Normal empty Movable zone start for each node Early memory node ranges node 0: [mem 0x0000000080000000-0x00000000ffffefff] Initmem setup node 0 [mem 0x0000000080000000-0x00000000ffffefff] On node 0 totalpages: 196608 DMA zone: 1536 pages used for memmap DMA zone: 0 pages reserved DMA zone: 196608 pages, LIFO batch:63 setup_cpuinfo: initialising setup_cpuinfo: Using full CPU PVR support ERROR: Microblaze HW_MUL-different for PVR and DTS wt_msr_noirq pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768 pcpu-alloc: [0] 0 Built 1 zonelists, mobility grouping on. Total pages: 195072 Kernel command line: console=ttyUL0,115200 Dentry cache hash table entries: 131072 (order: 7, 524288 bytes) Inode-cache hash table entries: 65536 (order: 6, 262144 bytes) Memory: 766124K/786432K available (4568K kernel code, 510K rwdata, 4416K rodata, 2886K init, 92K bss, 20308K reserved, 0K cma-reserved) Kernel virtual memory layout: * 0xffffe000..0xfffff000 : fixmap * 0xffffe000..0xffffe000 : early ioremap * 0xb0000000..0xffffe000 : vmalloc & ioremap NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0 irq-xilinx: mismatch in kind-of-intr param irq-xilinx: /amba_pl/interrupt-controller@41200000: num_irq=16, edge=0xffff05f0 /amba_pl/timer@41c00000: irq=1 clocksource: xilinx_clocksource: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604467 ns xilinx_timer_shutdown xilinx_timer_set_periodic sched_clock: 32 bits at 100MHz, resolution 10ns, wraps every 21474836475ns Calibrating delay loop... 49.35 BogoMIPS (lpj=246784) pid_max: default: 32768 minimum: 301 Mount-cache hash table entries: 2048 (order: 1, 8192 bytes) Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes) devtmpfs: initialized random: get_random_u32 called from bucket_table_alloc.isra.6+0x1e8/0x218 with crng_init=0 clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns futex hash table entries: 256 (order: -1, 3072 bytes) NET: Registered protocol family 16 jesd204: found 0 devices and 0 topologies clocksource: Switched to clocksource xilinx_clocksource NET: Registered protocol family 2 tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 4096 bytes) TCP established hash table entries: 8192 (order: 3, 32768 bytes) TCP bind hash table entries: 8192 (order: 3, 32768 bytes) TCP: Hash tables configured (established 8192 bind 8192) UDP hash table entries: 512 (order: 1, 8192 bytes) UDP-Lite hash table entries: 512 (order: 1, 8192 bytes) NET: Registered protocol family 1 RPC: Registered named UNIX socket transport module. RPC: Registered udp transport module. RPC: Registered tcp transport module. RPC: Registered tcp NFSv4.1 backchannel transport module. random: fast init done Skipping unavailable RESET gpio -2 (reset) workingset: timestamp_bits=30 max_order=18 bucket_order=0 jffs2: version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc. Block layer SCSI generic (bsg) driver version 0.4 loaded (major 252) io scheduler noop registered io scheduler deadline registered io scheduler cfq registered (default) io scheduler mq-deadline registered io scheduler kyber registered Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled 40600000.serial: ttyUL0 at MMIO 0x40600000 (irq = 5, base_baud = 0) is a uartlite console [ttyUL0] enabled brd: module loaded Xilinx SystemACE device driver, major=254 xilinx_spi 44a70000.axi_quad_spi: no CS gpios available libphy: Fixed MDIO Bus: probed xilinx_axienet 40c00000.ethernet: TX_CSUM 2 xilinx_axienet 40c00000.ethernet: RX_CSUM 2 xilinx_axienet 40c00000.ethernet: missing/invalid xlnx,addrwidth property, using default libphy: Xilinx Axi Ethernet MDIO: probed i2c /dev entries driver i2c i2c-0: Added multiplexed i2c bus 1 at24 2-0050: 256 byte 24c02 EEPROM, writable, 1 bytes/write i2c i2c-0: Added multiplexed i2c bus 2 i2c i2c-0: Added multiplexed i2c bus 3 i2c i2c-0: Added multiplexed i2c bus 4 i2c i2c-0: Added multiplexed i2c bus 5 i2c i2c-0: Added multiplexed i2c bus 6 i2c i2c-0: Added multiplexed i2c bus 7 i2c i2c-0: Added multiplexed i2c bus 8 pca954x 0-0075: registered 8 multiplexed busses for I2C switch pca9548 ad9528 spi0.0: spi0.0 supply vcc not found, using dummy regulator ad9528 spi0.0: Linked as a consumer to regulator.0 axi_adxcvr 44a50000.axi-ad9680-adxcvr: AXI-ADXCVR-RX (17.01.a) using CPLL on GTY 4 at 0x44A50000. Number of lanes: 4. axi_adxcvr 44a60000.axi-ad9152-adxcvr: AXI-ADXCVR-TX (17.01.a) using QPLL on GTY 4 at 0x44A60000. Number of lanes: 4. NET: Registered protocol family 17 ad9680 spi0.2: AD9680 PLL LOCKED cf_axi_adc 44a10000.axi-ad9680-hpc: ADI AIM (10.01.b) at 0x44A10000 mapped to 0x(ptrval), probed ADC AD9680 as MASTER cf_axi_dds 44a04000.axi-ad9152-hpc: Analog Devices CF_AXI_DDS_DDS MASTER (9.01.b) at 0x44A04000 mapped to 0x(ptrval), probed DDS AD9152 Freeing unused kernel memory: 2884K This architecture does not have kernel memory protection. Run /init as init process Starting logging: OK Initializing random number generator... random: dd: uninitialized urandom read (512 bytes read) done. Starting network: udhcpc: started, v1.27.2 net eth0: Promiscuous mode disabled. net eth0: Promiscuous mode disabled. udhcpc: sending discover xilinx_axienet 40c00000.ethernet eth0: Link is Down udhcpc: sending discover xilinx_axienet 40c00000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx udhcpc: sending discover udhcpc: sending discover udhcpc: sending select for 10.48.65.155 udhcpc: lease of 10.48.65.155 obtained, lease time 21600 deleting routers adding dns 10.32.51.110 adding dns 10.64.53.110 Starting dropbear sshd: random: dropbear: uninitialized urandom read (32 bytes read) OK Starting IIO Server Daemon Welcome to Buildroot buildroot login: root Password: #
Run the ifconfig command on your UART terminal and get your board IP
# ifconfig eth0 Link encap:Ethernet HWaddr 00:0A:35:00:00:00 inet addr:your_board_ip Bcast: Mask:255.255.255.0 UP BROADCAST RUNNING MTU:1500 Metric:1 RX packets:965 errors:0 dropped:0 overruns:0 frame:0 TX packets:3 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:126276 (123.3 KiB) TX bytes:1026 (1.0 KiB)
Check the available IIO devices (the following should be present):
# iio_info | grep iio:device iio:device3: axi-ad9152-hpc (buffer capable) iio:device1: ad9528 iio:device2: axi-ad9680-hpc (buffer capable) iio:device0: ad7291
Open IIO Scope application and type ip:board_ip in the URI tab
You should see two screens:
Analog Devices will provide limited online support for anyone using the reference design with Analog Devices components via the EngineerZone.