This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | |||
resources:eval:user-guides:ad-fmcdaq2-ebz:testing [04 May 2019 20:00] Mihai Bancisor [Creating an SD test card] |
resources:eval:user-guides:ad-fmcdaq2-ebz:testing [09 Jan 2021 00:32] Robin Getz user interwiki links |
||
---|---|---|---|
Line 23: | Line 23: | ||
This section requires checking the [[./hardware#downloads|schematics]]. Specifically, sheet 7 shows how the AD7291 is connected. 1% resistors connect various voltages, and things are divided down to ensure that the voltage levels don't exceed full scale. | This section requires checking the [[./hardware#downloads|schematics]]. Specifically, sheet 7 shows how the AD7291 is connected. 1% resistors connect various voltages, and things are divided down to ensure that the voltage levels don't exceed full scale. | ||
- | The explanation of how the valid ranges are calculated is similar to the same tests for the [[http://wiki.analog.com/resources/eval/user-guides/ad-fmcomms2-ebz/testing|FMComms boards]]. | + | The explanation of how the valid ranges are calculated is similar to the same tests for the [[/resources/eval/user-guides/ad-fmcomms2-ebz/testing|FMComms boards]]. |
==== Signals ==== | ==== Signals ==== | ||