Wiki

This version is outdated by a newer approved version.DiffThis version (18 Dec 2017 20:41) was approved by Charly El-Khoury.The Previously approved version (20 Jul 2015 14:49) is available.Diff

This is an old revision of the document!


AD-FMCDAQ2-EBZ Quick Start Guides

The Quick Start Guides provide a simple step by step instruction on how to do an initial system setup for the AD-FMCDAQ2-EBZ boards on various FPGA development boards. They will discuss how to program the bitstream, run a no-OS program or boot a Linux distribution.

Supported Carriers

The AD-FMCDAQ2-EBZ is, by definition a “FPGA mezzanine card” (FMC), that means it needs a carrier to plug into. The carriers we support are:

The supported OS are:

Board HDL Linux Software No-OS Software
Arria10 SoC Dev Kit v v v
Arria10 GX FPGA Dev Kit v v v
KC705 v v v
KCU105 v v v
VC707 v v v
ZC706 v v v

Hardware Setup

In most carriers, the AD-FMCDAQ2-EBZ board connects to the HPC connector (unless otherwise noted). The carrier setup requires power, UART (115200), ethernet (Linux), HDMI (if available) and/or JTAG (no-OS) connections. A typical setup is shown below.

resources/eval/user-guides/ad-fmcdaq2-ebz/quickstart.1503666621.txt.gz · Last modified: 25 Aug 2017 15:10 by Lars-Peter Clausen