This is an old revision of the document!
All the products described on this page include ESD (electrostatic discharge) sensitive devices. Electrostatic charges as high as 4000V readily accumulate on the human body or test equipment and can discharge without detection.
Although the boards feature ESD protection circuitry, permanent damage may occur on devices subjected to high-energy electrostatic discharges. Therefore, proper ESD precautions are recommended to avoid performance degradation or loss of functionality. This includes removing static charge on external equipment, cables, or antennas before connecting to the device.
Nios II Command Shell is used to program the FPGA. To run Nios II Command Shell navigate to C:\intelFPGA_pro\21.2\nios2eds and start Nios II Command Shell.bat. Windows Subsystem for Linux (WSL) needs to be installed in order to run Nios II Command Shell.
After starting the Command Shell, navigate to the path where the pre-build images are saved. For example:
ceshu@LADACE-L02:/mnt/c/intelFPGA_pro/21.2/nios2eds$ cd /mnt/c/Users/ladace/Downloads/a10gx_daq2_2019_r2/
To flash the bitfield pre-build image, nios2-configure-sof command is used. For example:
ceshu@LADACE-L02:/mnt/c/Users/ladace/Downloads/a10gx_daq2_2019_r2$ nios2-configure-sof daq2_a10gx.sof Searching for SOF file: in . daq2_a10gx.sof Info: ******************************************************************* Info: Running Quartus Prime Programmer Info: Command: quartus_pgm --no_banner --mode=jtag -o p;./daq2_a10gx.sof Info (213045): Using programming cable "USB-BlasterII [USB-1]" Info (213011): Using programming file ./daq2_a10gx.sof with checksum 0x312984DD for device 10AX115S2F45@1 Info (209060): Started Programmer operation at Thu Dec 9 15:10:50 2021 Info (209016): Configuring device index 1 Info (209017): Device 1 contains JTAG ID code 0x02E060DD Info (209007): Configuration succeeded -- 1 device(s) configured Info (209011): Successfully performed operation(s) Info (209061): Ended Programmer operation at Thu Dec 9 15:11:05 2021 Info: Quartus Prime Programmer was successful. 0 errors, 0 warnings Info: Peak virtual memory: 1829 megabytes Info: Processing ended: Thu Dec 9 15:11:05 2021 Info: Elapsed time: 00:00:22 Info: System process ID: 20500
To flash the Linux pre-build image, nios2-download command is used. For example:
ceshu@LADACE-L02:/mnt/c/Users/ladace/Downloads/a10gx_daq2_2019_r2$ nios2-download -g zImage Using cable "USB-BlasterII [USB-1]", device 1, instance 0x00 Pausing target processor: OK Initializing CPU cache (if present) OK Downloaded 5468KB in 6.1s (896.3KB/s) Verified OK Starting processor at address 0xC4000000
To start the Nios II Terminal use the following nios2-terminal.exe command. Example of console:
ceshu@LADACE-L02:/mnt/c/Users/ladace/Downloads/a10gx_daq2_2019_r2$ nios2-terminal.exe nios2-terminal: connected to hardware target using JTAG UART on cable nios2-terminal: "USB-BlasterII [USB-1]", device 1, instance 0 nios2-terminal: (Use the IDE stop button or Ctrl-C to terminate) Linux version 4.19.0-g17f4223 (jenkins@romlxbuild1.adlk.analog.com) (gcc version 8.3.1 20190416 (Altera 19.3 Build 222)) #1874 Tue Jul 27 14:44:52 IST 2021 On node 0 totalpages: 65536 Normal zone: 512 pages used for memmap Normal zone: 0 pages reserved Normal zone: 65536 pages, LIFO batch:15 pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768 pcpu-alloc: [0] 0 Built 1 zonelists, mobility grouping on. Total pages: 65024 Kernel command line: debug console=ttyJ0,115200 Dentry cache hash table entries: 32768 (order: 5, 131072 bytes) Inode-cache hash table entries: 16384 (order: 4, 65536 bytes) Sorting __ex_table... Memory: 247936K/262144K available (3795K kernel code, 465K rwdata, 4372K rodata, 3156K init, 106K bss, 14208K reserved, 0K cma-reserved) NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0 clocksource: nios2-clksrc: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604467 ns Calibrating delay loop (skipped), value calculated using timer frequency.. 200.00 BogoMIPS (lpj=400000) pid_max: default: 32768 minimum: 301 Mount-cache hash table entries: 1024 (order: 0, 4096 bytes) Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes) devtmpfs: initialized random: get_random_u32 called from bucket_table_alloc.isra.6+0x98/0x1e8 with crng_init=0 clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns futex hash table entries: 256 (order: -1, 3072 bytes) NET: Registered protocol family 16 jesd204: found 0 devices and 0 topologies clocksource: Switched to clocksource nios2-clksrc NET: Registered protocol family 2 tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 4096 bytes) TCP established hash table entries: 2048 (order: 1, 8192 bytes) TCP bind hash table entries: 2048 (order: 1, 8192 bytes) TCP: Hash tables configured (established 2048 bind 2048) UDP hash table entries: 256 (order: 0, 4096 bytes) UDP-Lite hash table entries: 256 (order: 0, 4096 bytes) NET: Registered protocol family 1 RPC: Registered named UNIX socket transport module. RPC: Registered udp transport module. RPC: Registered tcp transport module. RPC: Registered tcp NFSv4.1 backchannel transport module. random: fast init done workingset: timestamp_bits=30 max_order=16 bucket_order=0 jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc. Block layer SCSI generic (bsg) driver version 0.4 loaded (major 252) io scheduler noop registered io scheduler deadline registered io scheduler cfq registered (default) io scheduler mq-deadline registered io scheduler kyber registered 101814f0.serial: ttyJ0 at MMIO 0x101814f0 (irq = 2, base_baud = 0) is a Altera JTAG UART console [ttyJ0] enabled loop: module loaded spi_altera 10181400.spi: base (ptrval), irq 8 libphy: Fixed MDIO Bus: probed libphy: altera_tse: probed altera_tse 10181000.ethernet (unnamed net_device) (uninitialized): MDIO bus altera_tse-0: created altera_tse 10181000.ethernet: Altera TSE MAC version 19.3 at 0x10181000 irq 1/3 ad9680 spi0.2: Unrecognized CHIP_ID 0x0 iio iio:device0: SPI Read Verify failed (0x0) ad9523: probe of spi0.0 failed with error -5 ad9144 spi0.1: Unrecognized CHIP_ID 0xFF00 and CHIP_GRADE 0x0 NET: Registered protocol family 17 Freeing unused kernel memory: 3156K This architecture does not have kernel memory protection. Run /init as init process Starting logging: OK Initializing random number generator... random: dd: uninitialized urandom read (512 bytes read) done. Starting network: OK altera_tse 10181000.ethernet eth0: device MAC address b2:94:3d:6e:11:8f altera_tse 10181000.ethernet eth0: TSE revision 1303 altera_tse 10181000.ethernet eth0: PCS PHY ID: 0x00000000 altera_tse 10181000.ethernet eth0: SGMII PCS block initialised OK altera_tse 10181000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx Network cable is plugged udhcpc: started, v1.25.0 udhcpc: sending discover udhcpc: sending select for 10.48.65.150 udhcpc: lease of 10.48.65.150 obtained, lease time 21600 deleting routers adding dns 10.32.51.110 adding dns 10.64.53.110 inet addr:10.48.65.150 Bcast:10.48.65.255 Mask:255.255.255.0 Starting dropbear sshd: random: dropbear: uninitialized urandom read (32 bytes read) OK Starting IIO Server Daemon Welcome to Buildroot buildroot login:
To connect the board to IIO Scope start the IIO Oscilloscope application and go to Settings menu and then press Connect. From Select or Discover libIIO Context select Manual and enter the URI in the following format ip:<your_board_ip> Press the Refresh button and then Connect.
To determine the IP of the board, in Nios II Command Shell login using root and password analog. Then run the ifconfig command. For example:
ifconfig eth0 Link encap:Ethernet HWaddr B2:94:3D:6E:11:8F inet addr:10.48.65.132 Bcast:10.48.65.255 Mask:255.255.255.0 UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1 RX packets:96785 errors:0 dropped:13841 overruns:0 frame:0 TX packets:13511 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:17852315 (17.0 MiB) TX bytes:8770953 (8.3 MiB) Memory:10181000-101813ff lo Link encap:Local Loopback inet addr:127.0.0.1 Mask:255.0.0.0 UP LOOPBACK RUNNING MTU:65536 Metric:1 RX packets:0 errors:0 dropped:0 overruns:0 frame:0 TX packets:0 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
To plot the captured waveforms go to File menu then click New Plot. Select the channels to plot and then click Capture / Stop button.
Analog Devices will provide limited online support for anyone using the reference design with Analog Devices components via the EngineerZone.