Wiki

This version (28 Jan 2021 19:58) was approved by Robin Getz.The Previously approved version (27 Nov 2017 11:51) is available.Diff

AD-FMCDAQ2-EBZ Hardware

Picture and Main components

Outline

For those that don't want to load up the Allegro viewer, here is a basic outline/component placements of the board.

Size

The size of the board (not including the SMA connectors, which project beyond the edge of the board) is 3.12 inches by 2.72 inches (or about 79mm x 69mm).
















Downloads

resources/eval/user-guides/ad-fmcdaq2-ebz/hardware.txt · Last modified: 28 Jan 2021 19:56 by Robin Getz