Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:eval:user-guides:ad-fmcdaq2-ebz:clocking [14 Sep 2017 11:04]
Lars-Peter Clausen [Replacing the Crystal Oscillator] typo
resources:eval:user-guides:ad-fmcdaq2-ebz:clocking [19 Jan 2018 10:14]
Alexandru Ardelean rename xcomm_zynq -> master
Line 128: Line 128:
 On Linux the default clock configuration is supplied through the [[https://​www.devicetree.org/​|devicetree]]. On Linux the default clock configuration is supplied through the [[https://​www.devicetree.org/​|devicetree]].
  
-The devicetree file that is used for the AD-FMCDAQ2-EBZ and contains the clock configuration is called [[linux.github>​xcomm_zynq?​arch/​arm/​boot/​dts/​adi-daq2.dtsi|adi-daq2.dtsi]]. This file contains nodes for the [[linux.github>​xcomm_zynq?​arch/​arm/​boot/​dts/​adi-daq2.dtsi#​L8|AD9523-1]],​ the [[linux.github>​xcomm_zynq?​arch/​arm/​boot/​dts/​adi-daq2.dtsi#​L105|AD9144]] and the [[linux.github>​xcomm_zynq?​arch/​arm/​boot/​dts/​adi-daq2.dtsi#​L120|AD9680]]. Each node contains properties that describe the hardware setup and provide default configuration parameters. For information on how to edit devicetree please see [[:​resources:​eval:​user-guides:​ad-fmcomms2-ebz:​software:​linux:​zynq_tips_tricks#​customizing_the_device_tree_on_the_target|Tips & Tricks - Customizing the device tree on the target]].+The devicetree file that is used for the AD-FMCDAQ2-EBZ and contains the clock configuration is called [[linux.github>​master?​arch/​arm/​boot/​dts/​adi-daq2.dtsi|adi-daq2.dtsi]]. This file contains nodes for the [[linux.github>​master?​arch/​arm/​boot/​dts/​adi-daq2.dtsi#​L8|AD9523-1]],​ the [[linux.github>​master?​arch/​arm/​boot/​dts/​adi-daq2.dtsi#​L105|AD9144]] and the [[linux.github>​master?​arch/​arm/​boot/​dts/​adi-daq2.dtsi#​L120|AD9680]]. Each node contains properties that describe the hardware setup and provide default configuration parameters. For information on how to edit devicetree please see [[:​resources:​eval:​user-guides:​ad-fmcomms2-ebz:​software:​linux:​zynq_tips_tricks#​customizing_the_device_tree_on_the_target|Tips & Tricks - Customizing the device tree on the target]].
  
 To change the clocking configuration the properties of the AD9523-1 node can be modified. The following lists the most important properties for the AD-FMCDAQ2-EBZ and their corresponding hardware setting. The function of each of these settings and how to choose their value has been discussed above. For more information refer to the [[:​resources:​tools-software:​linux-drivers:​iio-pll:​ad9523|AD9523-1 driver documenation]]. To change the clocking configuration the properties of the AD9523-1 node can be modified. The following lists the most important properties for the AD-FMCDAQ2-EBZ and their corresponding hardware setting. The function of each of these settings and how to choose their value has been discussed above. For more information refer to the [[:​resources:​tools-software:​linux-drivers:​iio-pll:​ad9523|AD9523-1 driver documenation]].
resources/eval/user-guides/ad-fmcdaq2-ebz/clocking.txt · Last modified: 19 Jan 2018 10:14 by Alexandru Ardelean