Wiki

This version is outdated by a newer approved version.DiffThis version (16 Nov 2015 19:27) was approved by rejeesh kutty.

This is an old revision of the document!


AD-FMCADC7-EBZ FMC Board

Introduction

The AD-FMCADC4-EBZ is a high speed four channel data acquisition board featuring two AD9680 dual channel ADC at 1000 MSPS (1240 MSPS) and four ADA4961 ADA4961 low distortion, 3.2 GHz, RF DGA driving each converter. The FMC form factor supports the JESD204B high speed serial interface. All clocking and channel synchronization is provisioned on-board using the AD9528 AD9528 clock generator. This board meets most of the FMC specifications in terms of mechanical size, mounting hole locations etc., for further details, please refer to the FMC specification.

Although this board does meet most of the FMC specifications, it is not meant as a commercial off the shelf (COTS) board. If a commercial, ready to go integrate product is required, please refer to one of the many FMC manufacturers.

ADI also provides reference designs (HDL and software) for this board to work with commonly available Altera and Xilinx development boards.

Hardware

The AD-FMCADC4-EBZ board's primary purpose is to demonstrate the capabilities of the devices on board quickly and easily by providing a seamless interface to an FMC carrier platform and running the reference design on the carrier FPGA. The board is designed to self power and self clock when connected to the FMC carrier. The analog signals (up to four) are connected to J301A, J301B, J301C and J301D. This rapid prototyping board can also be synchronized across channels.

Devices

The FMC board includes the following products by Analog Devices:

  • AD9680 14-bit dual channel ADC with sampling speeds of up to 1250 MSPS, with a JESD204B digital interface.
  • ADA4961 Low Distortion, 3.2 GHz, RF Digital Gain Amplifier.
  • AD9528 JESD204B Clock Generator with 14 LVDS Outputs
  • ADP2384 20 V, 4 A, Synchronous, Step-Down DC-to-DC Regulator
  • ADP7104 is a 20V, 500mA, low noise, CMOS LDO
  • ADM7154 600 mA, Ultra Low Noise, High PSRR, RF Linear Regulator
  • ADM7172 6.5 V, 2 A, Ultralow Noise, High PSRR, Fast Transient Response CMOS LDO
  • ADP1741 is a 2A, low Vin, low dropout, CMOS linear regulator

                                                 Top View

                                                 Bottom View

Clocking

The AD-FMCADC4-EBZ includes an on-board 80MHz reference oscillator from Crystek. This feature can be disconnected and an external reference can be applied through J901. When referencing the schematic make sure the proper component changes are made in order to directly route the input into the AD9528.

Analog Front End

The AD-FMCADC4-EBZ uses a passive front end designed for very wide bandwidth. A single ended input needs to be provided to the analog inputs mentioned earlier. A 1:2 impedance ratio broadband balun then converts the input signal differentially to the ADA4961 inputs and has a 1.6GHz bandwidth at -3dB. Each channel amplifier can be adjusted independently in terms of gain.

Revision A

The revision A board supports amplifier gain control via spi. After power-up, the gain of the amplifier defaults to an attenuated state. Use a low jitter, low noise signal source with a level at -20dBm to the analog inputs (J301-A/B/C/D). Apply a signal source no greater than -10dBm to achieve full-scale of the converter when maximum gain of the amplifier is applied.

Running No-OS Application & Changing Sampling Rate to 1.24GHz

The HDL reference design is built around a processor as in an embedded system. You may use either Linux or No-OS software to demonstrate the design (details in the downloads section). In order to run the HDL with the No-OS application, one need to build the HDL bit file and software elf file.

At the time of this writing, we are using the 'dev' branch for both. The HDL user guide contains the instructions to build the bit file. Please make sure you use the 'dev' branch (checkout dev right after cloning).

Once the bit file is ready, follow these instructions to build the elf file. This assumes you are following our directory structures. If you are not, just get the idea from here and port it to your environment. However you have to figure out things on your own.

  1. Clone No-OS repository
  2. Checkout the 'dev' branch (git checkout dev)
  3. Change the directory to `ad-fmcadc4-ebz/zc706`.
  4. Make the elf file by running `make HDF-FILE=<HDL-REPO>/projects/fmcadc4/zc706/fmcadc4_zc706.sdk/system_top.hdf`

The make will build the default 'hello-world', but we only need the bsp and I am no fan of eclipse, hence this method. If you are more comfortable with the GUI, import all the files (or folders) that the make uses.

A typical run looks like this:

[~/github/noos/ad-fmcadc4-ebz/zc706]> make HDF-FILE=~/github/hdl/projects/fmcadc4/zc706/fmcadc4_zc706.sdk/system_top.hdf 
xsct -s ../../scripts/xilinx_xsct.tcl ~/github/hdl/projects/fmcadc4/zc706/fmcadc4_zc706.sdk/system_top.hdf >> xilinx_xsct.log 2>&1
                                                                                                                                                                                                 
arm-xilinx-eabi-gcc -DXILINX -Ibsp/ps7_cortexa9_0/include -I.. -I../../common_drivers/adc_core -I../../common_drivers/jesd204b_gt -I../../common_drivers/jesd204b_v51 -I../../common_drivers/xilinx_platform_drivers -I../../drivers/ad9528 -I../../drivers/ad9680 -Os -ffunction-sections -fdata-sections -o zc706.elf sw/src/platform.c ../ad_fmcadc4_ebz.c ../../common_drivers/adc_core/adc_core.c ../../common_drivers/jesd204b_gt/jesd204b_gt.c ../../common_drivers/jesd204b_v51/jesd204b_v51.c ../../common_drivers/xilinx_platform_drivers/platform_drivers.c ../../drivers/ad9528/ad9528.c ../../drivers/ad9680/ad9680.c -Lbsp/ps7_cortexa9_0/lib/ -Tsw/src/lscript.ld -Wl,--start-group,-lxil,-lgcc,-lc,--end-group
[~/github/noos/ad-fmcadc4-ebz/zc706]

Start an UART terminal.

[USB0]
port	= /dev/ttyUSB0
speed	= 115200
bits	= 8
stopbits	= 1
parity	= none
crlfauto	= True ## if not set, expect non-aligned text

[~/github/noos/ad-fmcadc4-ebz/zc706]> gtkterm -c USB0 &

The folder contains a zc706.tcl file that you can launch with xmd. You can also run it using Vivado or SDK - up to you.

[~/github/noos/ad-fmcadc4-ebz/zc706]> xmd -tcl zc706.tcl 
rlwrap: warning: your $TERM is 'xterm' but rlwrap couldn't find it in the terminfo database. Expect some problems.
                                                                                                                                                                                                 
 Xilinx Microprocessor Debugger (XMD) Engine
 XMD v2015.2 (64-bit)
   SW Build 1266856 on Fri Jun 26 16:35:25 MDT 2015
    ** Copyright 1986-2015 Xilinx, Inc. All Rights Reserved.

Executing user script : zc706.tcl
Configuring Device 2 (xc7z045) with Bitstream -- hw/system_top.bit                                                                                                                               
....................10...................20...................30....................40...................50...................60....................70...................80...................90....................Done
Successfully downloaded bit file.

JTAG chain configuration
--------------------------------------------------
Device   ID Code        IR Length    Part Name
 1       4ba00477           4        arm_dap
 2       23731093           6        xc7z045


JTAG chain configuration
--------------------------------------------------
Device   ID Code        IR Length    Part Name
 1       4ba00477           4        arm_dap
 2       23731093           6        xc7z045

--------------------------------------------------
Enabling extended memory access checks for Zynq.
Writes to reserved memory are not permitted and reads return 0.
To disable this feature, run "debugconfig -memory_access_check disable".

--------------------------------------------------

CortexA9 Processor Configuration
-------------------------------------
Version.............................0x00000003
User ID.............................0x00000000
No of PC Breakpoints................6
No of Addr/Data Watchpoints.........4

Connected to "arm" target. id = 64
Starting GDB server for "arm" target (id = 64) at TCP port no 1234
Processor stopped

Processor Reset .... DONE                                                                                                                                                                        
Downloading Program -- zc706.elf
        section, .text: 0x00100000-0x0010656b
        section, .init: 0x0010656c-0x00106583
        section, .fini: 0x00106584-0x0010659b
        section, .rodata: 0x0010659c-0x00106927
        section, .data: 0x00106928-0x00106e9b
        section, .eh_frame: 0x00106e9c-0x00106e9f
        section, .mmu_tbl: 0x00108000-0x0010bfff
        section, .ARM.exidx: 0x0010c000-0x0010c007
        section, .init_array: 0x0010c008-0x0010c00f
        section, .fini_array: 0x0010c010-0x0010c013
        section, .bss: 0x0010c014-0x0010c0a7
        section, .heap: 0x0010c0a8-0x0010e0af
        section, .stack: 0x0010e0b0-0x001118af
Download Progress..10.20.30.40.50.60.70.80.90.Done
Setting PC with Program Start Address 0x00100000
Processor started. Type "stop" to stop processor

RUNNING> Disconnected from Target 64

Disconnected from Target 352

The following messages should appear on the terminal.

AD9528 successfully initialized.
AD9680 PLL is locked.
AD9680 successfully initialized.
AD9680 PLL is locked.
AD9680 successfully initialized.
JESD204B successfully initialized.
ADC Core Initialized (1000 MHz).
ADC Core Initialized (1000 MHz).
Initialization done.

Capture done.

A brief background information on what is happening. Let's look at the No-OS main function. First, it configures and sets the GPIO based on the board.

	adc4_gpio_ctl(GPIO_DEVICE_ID);

The clock chip is programmed to output the desired clocks and sys-ref signals. The default setting is 1GHz for the AD9680 and 500MHz for the FPGA.

	 ad9528_setup(SPI_DEVICE_ID, 0, ad9528_pdata_lpc);

The transceiver cores are initialized. Here only DRP access is possible. If you are planning to change the transceivers, this is where they should be.

	 jesd204b_gt_initialize(FMCADC4_GT_BASEADDR, 8);

The AD9680 devices are initialized (checking the PLL status)

	 ad9680_setup(SPI_DEVICE_ID, 1);
	 ad9680_setup(SPI_DEVICE_ID, 2);

The design uses Xilinx's JESD IP- it needs to be programmed to match the device settings (frame count, byte count, scrambling and such).

	 jesd204b_setup(AD9680_JESD_BASEADDR, jesd204b_st);

After the above setup, bring the transceivers up, here we check for everything on the link, starting from the PLL locked to SYNC deasserted.

 	jesd204b_gt_setup(ad9680_gt_link);

The individual AD9680 cores are brought out of reset.

	 adc_setup(ad9680_0, 2);
	 adc_setup(ad9680_1, 2);

The ADC has a PRBS generator at the sample level that can be monitored in the FPGA. This is a robust way to confirming the link status. The software monitors this and reports any errors.

This is setting the PRBS generator in the device.

	ad9680_spi_write(1, AD9680_REG_DEVICE_INDEX, 0x3);
 	ad9680_spi_write(1, AD9680_REG_ADC_TEST_MODE, 0x05);
 	ad9680_spi_write(1, AD9680_REG_OUTPUT_MODE, 0);
	ad9680_spi_write(2, AD9680_REG_DEVICE_INDEX, 0x3);
	ad9680_spi_write(2, AD9680_REG_ADC_TEST_MODE, 0x05);
	ad9680_spi_write(2, AD9680_REG_OUTPUT_MODE, 0);

This is setting the PRBS monitors in the FPGA.

	adc_pn_mon(ad9680_0, 2, 1);
	adc_pn_mon(ad9680_1, 2, 1);

If you don't see any other messages in the UART other than the ones mentioned above- all is well. You can open up Vivado and see things in ILA also.

Let's see now how we can change the sampling rate to 1.24 GHz. The AD9680 maximum sampling rate is 1.25GHz. However the board uses a 80MHz crystal as the reference clock to AD9528. Unless you change it, this limits the maximum clock output on the banks to 1.24GHz. Also note that the Kintex 7 SOC on ZC706 is a -2 device. The maximum lane rate is limited to 10Gbps. However, it should be possible to over clock the transceiver (but do so at your own risk). Officially, you must get a -3 device to run the link at 12.4Gbps.

Going back to our program.

#ifdef MODE_1_24G
	ad9528_pdata_lpc.pll2_ndiv_a_cnt = 1;
	ad9528_pdata_lpc.pll2_ndiv_b_cnt = 23;
	ad9528_pdata_lpc.pll2_n2_div = 31;
	ad9528_pdata_lpc.pll2_vco_diff_m1 = 3;
#endif

Let's define that macro somewhere on that file.

[~/github/noos/ad-fmcadc4-ebz/zc706]> gitdiff.pl ../ad_fmcadc4_ebz.c 
71a72
> #define MODE_1_24G

And re-run the make.

[~/github/noos/ad-fmcadc4-ebz/zc706]> make HDF-FILE=~/github/hdl/projects/fmcadc4/zc706/fmcadc4_zc706.sdk/system_top.hdf 
arm-xilinx-eabi-gcc -DXILINX -Ibsp/ps7_cortexa9_0/include -I.. -I../../common_drivers/adc_core -I../../common_drivers/jesd204b_gt -I../../common_drivers/jesd204b_v51 -I../../common_drivers/xilinx_platform_drivers -I../../drivers/ad9528 -I../../drivers/ad9680 -Os -ffunction-sections -fdata-sections -o zc706.elf sw/src/platform.c ../ad_fmcadc4_ebz.c ../../common_drivers/adc_core/adc_core.c ../../common_drivers/jesd204b_gt/jesd204b_gt.c ../../common_drivers/jesd204b_v51/jesd204b_v51.c ../../common_drivers/xilinx_platform_drivers/platform_drivers.c ../../drivers/ad9528/ad9528.c ../../drivers/ad9680/ad9680.c -Lbsp/ps7_cortexa9_0/lib/ -Tsw/src/lscript.ld -Wl,--start-group,-lxil,-lgcc,-lc,--end-group

The UART should now show this.

AD9528 successfully initialized.
AD9680 PLL is locked.
AD9680 successfully initialized.
AD9680 PLL is locked.
AD9680 successfully initialized.
JESD204B successfully initialized.
ADC Core Initialized (1240 MHz).
ADC Core Initialized (1240 MHz).
Initialization done.

Capture done.

The clocks reported by the core is 1240MHz instead of the previous 1000MHz. There are no error messages and PRBS locks. This is all there is to it. There is no need for HDL modifications. However, if you ran into trouble here are a couple of things to try.

  • If you have ran this back to back- try running 1.24GHz option from power up.
  • Modify the HDL to use a -3 device and change the constraints to run at 12.40Gbps
  • Upgrade the device on board to a -3 device.

Here is the UART window screen capture.

FMCADC4-UART

The application leaves the device in a ramp pattern, and if you are looking at the data using ILA should see it. If you would like to switch it to the analog input, do the following. In this case I am changing only the fourth channel (SMA - J301D).

	ad9680_spi_write(1, AD9680_REG_DEVICE_INDEX, 0x3);
	ad9680_spi_write(1, AD9680_REG_ADC_TEST_MODE, 0x0F);
	ad9680_spi_write(1, AD9680_REG_OUTPUT_MODE, 0x1);

	ad9680_spi_write(2, AD9680_REG_DEVICE_INDEX, 0x3);
	ad9680_spi_write(2, AD9680_REG_ADC_TEST_MODE, 0x0F);
	ad9680_spi_write(2, AD9680_REG_OUTPUT_MODE, 0x1);

	ad9680_spi_write(2, AD9680_REG_DEVICE_INDEX, 0x2);
	ad9680_spi_write(2, AD9680_REG_ADC_TEST_MODE, 0x00);
	ad9680_spi_write(2, AD9680_REG_OUTPUT_MODE, 0x1);
        adc_write(ad9680_1, ADC_REG_CHAN_CNTRL(1), 0x51);

Here is the ILA plot screen capture.

FMCADC4-ILA

Downloads (Hardware)

Downloads (HDL)

Projects list and dependencies for master

AD40XXFMC

AD469XFMC

AD5758SDZ

AD5766SDZ

AD6676EVB

AD7134FMC

AD738xFMC

AD7405FMC

AD7616SDZ

AD77681EVB

AD7768EVB

AD9081FMCAEBZ

AD9082FMCAEBZ

AD9083EVB

AD9208DUALEBZ

AD9265FMC

AD9434FMC

AD9467FMC

AD9656FMC

AD9739AFMC

ADFMCLIDAR1EBZ

ADAQ7980SDZ

ADRV9001

ADRV9008/9

ADRV9371

ADV7511OnBoard

ADV7513OnBoard

Hardware Project Carriers Resource Utilization Library Cores
ADV7513 adv7513 de10nano NA axi_dmac
axi_hdmi_tx
util_axis_fifo

ARRadio

Hardware Project Carriers Resource Utilization Library Cores
ARRadio arradio c5soc NA axi_ad9361
axi_dmac
axi_sysid
sysid_rom
util_axis_fifo
util_cdc
util_cpack2
util_rfifo
util_upack2

CN0363

CN0501

Hardware Project Carriers Resource Utilization Library Cores
CN0501 cn0501 coraz7s cn0501_coraz7s axi_dmac
axi_generic_adc
axi_sysid
sysid_rom
util_axis_fifo
util_cdc

CN0506MII

CN0506RGMII

CN0506RMII

Hardware Project Carriers Resource Utilization Library Cores
CN0506 cn0506_rmii zc706 NA axi_clkgen
zcu102 NA axi_dmac
zed NA axi_hdmi_tx
axi_i2s_adi
axi_spdif_tx
axi_sysid
sysid_rom
util_axis_fifo
util_cdc

CN0540

DACFMCEBZ

FMCDAQ2

FMCDAQ3

FMCADC2/FMCADC3

FMCADC5

FMCJESDADC1

FMCOMMS11

FMCOMMS2/FMCOMMS3/FMCOMMS4

FMCOMMS5

FMCOMMS8

FMCIMAGEONG

Help & Support

Help & Support

Downloads (Linux)

resources/eval/user-guides/ad-fmcadc7-ebz.1447698227.txt.gz · Last modified: 16 Nov 2015 19:23 by rejeesh kutty