Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:eval:user-guides:ad-fmcadc5-ebz [20 Mar 2018 17:03]
AdrianC Cleanup
resources:eval:user-guides:ad-fmcadc5-ebz [14 Feb 2019 10:21] (current)
AdrianC Fixed broken links
Line 2: Line 2:
  
 ===== Introduction ===== ===== Introduction =====
-{{  :​resources:​eval:​user-guides:​ad-fmcadc5-ebz:​ad-fmcadc5-ebz.jpg?​400|}} The [[http://​www.xilinx.com/​products/​boards-and-kits/​1-5l1boj.html|AD-FMCADC5-EBZ]] is a high speed single channel data acquisition board featuring two [[adi>​AD9625]] ADCs. The board is provisioned to sample the single input at an effective sampling rate of 5GSPS, with both the ADCs running at 2.5GHz and sampling at both edges (the clocks are 180 out of phase to each other). The board is a variant of [[http://www.fidus.com/analog-digital-converters|FSF-AD15000A]] from Fidus Systems Inc.+{{  :​resources:​eval:​user-guides:​ad-fmcadc5-ebz:​ad-fmcadc5-ebz.jpg?​400|}} The [[adi>AD-FMCADC5-EBZ|AD-FMCADC5-EBZ]] is a high speed single channel data acquisition board featuring two [[adi>​AD9625]] ADCs. The board is provisioned to sample the single input at an effective sampling rate of 5GSPS, with both the ADCs running at 2.5GHz and sampling at both edges (the clocks are 180 out of phase to each other). The board is a variant of [[https://​fidus.com/​fmcs/|FSF-AD15000A]] from Fidus Systems Inc.
  
 Although this board does meet most of the FMC specifications,​ it is not meant as a [[wp>​Commercial_off-the-shelf|commercial off the shelf]] (COTS) board. If a commercial, ready to go integrate product is required, please refer to one of the many FMC manufacturers. Although this board does meet most of the FMC specifications,​ it is not meant as a [[wp>​Commercial_off-the-shelf|commercial off the shelf]] (COTS) board. If a commercial, ready to go integrate product is required, please refer to one of the many FMC manufacturers.
Line 22: Line 22:
  
 The AD-FMCADC5-EBZ uses a 2.5GHz crystal. The two AD9625 devices are clocked from the same clock source, but 180 degrees out of phase. The AD-FMCADC5-EBZ uses a 2.5GHz crystal. The two AD9625 devices are clocked from the same clock source, but 180 degrees out of phase.
- 
-==== Analog Front End ==== 
  
 ===== Running No-OS Application & Achieving Interleaving at 5GSPS ===== ===== Running No-OS Application & Achieving Interleaving at 5GSPS =====
Line 39: Line 37:
   - Make the elf file by running `make HDF-FILE=<​HDL-REPO>/​projects/​fmcadc5/​vc707/​fmcadc5_vc707.sdk/​system_top.hdf`   - Make the elf file by running `make HDF-FILE=<​HDL-REPO>/​projects/​fmcadc5/​vc707/​fmcadc5_vc707.sdk/​system_top.hdf`
  
-The make will build the default '​hello-world',​ but we only need the bsp and I am no fan of eclipse, ​hence this method. If you are more comfortable with the GUI, import all the files (or folders) that the make uses.+The make will build the default '​hello-world',​ but we only need the bsp and I am no fan of eclipse, ​therefore ​this method. If you are more comfortable with the GUI, import all the files (or folders) that the make uses.
  
 A typical run looks like this: A typical run looks like this:
Line 383: Line 381:
  
 <WRAP center round download>​ <WRAP center round download>​
-  * AD-FMCADC5-EBZ No-OS - https://​github.com/​analogdevicesinc/​no-OS/​tree/​master/​ad-fmcadc5-ebz+  * AD-FMCADC5-EBZ No-OS - https://​github.com/​analogdevicesinc/​no-OS/​tree/​master/​fmcadc5
 </​WRAP>​ </​WRAP>​
  
  
resources/eval/user-guides/ad-fmcadc5-ebz.txt · Last modified: 14 Feb 2019 10:21 by AdrianC