Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision |
resources:eval:user-guides:ad-fmcadc4-ebz [13 Mar 2018 13:53] – 2017_r1 - Updates (remove ILA and 1.24G config) Andrei Grozav | resources:eval:user-guides:ad-fmcadc4-ebz [28 Oct 2019 19:38] – add note Robin Getz |
---|
====== AD-FMCADC4-EBZ FMC Board ====== | ====== AD-FMCADC4-EBZ FMC Board ====== |
| |
===== Introduction ===== | ===== Introduction ===== |
| |
| <WRAP important>The [[adi>EVAL-AD-FMCADC4-EBZ]] board has been retired, and is no longer available for sale. It has been removed from the HDL and software repository, but is still available in the history. |
| </WRAP> |
| |
The [[adi>EVAL-AD-FMCADC4-EBZ]] is a high speed four channel data acquisition board featuring two [[adi>AD9680]] dual channel ADC at 1000 MSPS (1240 MSPS) and four ADA4961 [[adi>ADA4961]] low distortion, 3.2 GHz, RF DGA driving each converter. The FMC form factor supports the JESD204B high speed serial interface. All clocking and channel synchronization is provisioned on-board using the AD9528 [[adi>AD9528]] clock generator. This board meets most of the FMC specifications in terms of mechanical size, mounting hole locations etc., for further details, please refer to the FMC specification. | The [[adi>EVAL-AD-FMCADC4-EBZ]] is a high speed four channel data acquisition board featuring two [[adi>AD9680]] dual channel ADC at 1000 MSPS (1240 MSPS) and four ADA4961 [[adi>ADA4961]] low distortion, 3.2 GHz, RF DGA driving each converter. The FMC form factor supports the JESD204B high speed serial interface. All clocking and channel synchronization is provisioned on-board using the AD9528 [[adi>AD9528]] clock generator. This board meets most of the FMC specifications in terms of mechanical size, mounting hole locations etc., for further details, please refer to the FMC specification. |