Wiki

This version (28 Aug 2015 13:11) was approved by Dragos Bogdan.The Previously approved version (28 Aug 2015 08:37) is available.Diff

AD-FMCADC3-EBZ Quick Start Guides

The Quick Start Guides provide a simple step by step instruction on how to do an initial system setup for the AD-FMCADC3-EBZ boards on various FPGA development boards. They will discuss how to program the bitstream, run a no-OS program or boot a Linux distribution.

Supported Carriers

The AD-FMCADC3-EBZ is, by definition a “FPGA mezzanine card” (FMC), that means it needs a carrier to plug into. The carriers we support are:

Board AD-FMCADC3-EBZ
VC707 v
ZC706 v

The supported OS are:

Board HDL Linux Software No-OS Software
VC707 v v -
ZC706 v v -

Hardware Setup

In most carriers, the AD-FMCADC3-EBZ board connects to the HPC connector (unless otherwise noted). The carrier setup requires power, UART (115200), ethernet (Linux), HDMI (if available) and/or JTAG (no-OS) connections. A typical setup is shown below.

resources/eval/user-guides/ad-fmcadc3-ebz/quickstart.txt · Last modified: 28 Aug 2015 13:10 by Dragos Bogdan