Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision |
resources:eval:user-guides:ad-96tof1-ebz [02 Oct 2019 10:15] – [Application Development] Andrei Cozma | resources:eval:user-guides:ad-96tof1-ebz [17 Oct 2019 23:27] – [Hardware Platform] Andrei Cozma |
---|
| |
Designed using a modular approach, the 3D ToF hardware prototyping platform enables connectivity to the [[https://www.96boards.org/|96Boards]] development boards suite. There is also a Raspberry PI camera connector that allows it to connect to any compatible system. Data is fed from the 3D camera to the host processor via 2 lane MIPI-CSI interface at frame rates up to 30fps. The system has full software support for data processing on the embedded processor platform as well as for USB, Ethernet or Wi-Fi to connect to a host computer, this flexibility enables evaluation across a wide range of use cases and environments. | Designed using a modular approach, the 3D ToF hardware prototyping platform enables connectivity to the [[https://www.96boards.org/|96Boards]] development boards suite. There is also a Raspberry PI camera connector that allows it to connect to any compatible system. Data is fed from the 3D camera to the host processor via 2 lane MIPI-CSI interface at frame rates up to 30fps. The system has full software support for data processing on the embedded processor platform as well as for USB, Ethernet or Wi-Fi to connect to a host computer, this flexibility enables evaluation across a wide range of use cases and environments. |
| |
| The system can be mounted on a [[https://www.manfrotto.com/global/pixi-mini-tripod-black-mtpixi-b/|tripod]] using the metal piece attached to the camera board. |
| |
^ Range ^ | ^ Range ^ |