This is an old revision of the document!
Nvidia Xavier NX User Guide
Setting up the system
Required hardware
Modifying the AD-96TOF1-EBZ to work with the Nvidia Xavier NX
All changes required for RPi are applicable to Nvidia Xavier NX. So please follow the instructions presented here: Raspberry Pi User Guide
Prepare SD card
Power on sequence
Plug the
SD card into the Nvidia Xavier NX
SD card slot
Connect the HDMI cable from the monitor to the Jetson HDMI connector
Connect the camera cable between the J1 connector of Jetson Xavier NX and the P1 connector of the ToF board
Connect a
USB mouse and keyboard to the Xavier NX
connect the 5V power supply to the camera board and set the camera power switch S2 to on. Once the camera board is powered up the DS1 LED will turn on
connect the 9V-19V power supply to the Xavier NX. Once power is connected to the Jetson the system will boot the Linux
OS from the
SD card.
Password for “analog” user is “analog”. This user has sudo rights
Power off sequence
Troubleshooting
Linux does not boot
The
SD card is corrupted and this prevents the system from booting. Reflash the
SD card or check generated devicetree or kernel image
Running the evaluation application
This example demonstrates how to capture data from the TOF system on the Nvidia Xavier NX and display it using OpenCV.