Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:eval:user-guides:ad-96tof1-ebz:ug_xavier_nx [16 Sep 2021 15:21]
Septimiu Vana [Prepare SD card]
resources:eval:user-guides:ad-96tof1-ebz:ug_xavier_nx [17 Dec 2021 13:01]
Septimiu Vana Add point cloud description
Line 46: Line 46:
 ===== Running the evaluation application ===== ===== Running the evaluation application =====
  
-[[https://​github.com/​analogdevicesinc/​aditof_sdk/​tree/​master/​examples/​aditof-demo | This example]] demonstrates how to capture data from the TOF system on the Nvidia ​Xavier NX and display it using OpenCV. ​+[[https://​github.com/​analogdevicesinc/​aditof_sdk/​tree/​master/​examples/​aditof-demo | This example]] demonstrates how to capture data from the TOF system on the Nvidia ​jetson ​and display it using OpenCV. ​
  
-{{navigation AD-96TOF1-EBZ#none#.:|Overview#​none#​}}+Once Linux boots you'll see on the HDMI monitor the Linux desktop and on the top left corner a shortcut to the evaluation application. Double clicking on the icon will start the evaluation application. A console window will open to show the application'​s status and, after a few seconds, the evaluation application GUI will be displayed. 
 + 
 +{{:​resources:​eval:​user-guides:ad-96tof1-ebz:​aditof_demo.png|}} 
 + 
 +When starting the application,​ a terminal window will open to display status messages (also warning and error messages, in case there are any issues). Shorty the main window will show up. 
 + 
 +The evaluation application allows to do live streaming of depth and IR data as well as recording the depth and IR data and playing back from a file. The depth data is displayed as a color map ranging from warm to cold colors as the distance from the camera increases. A point in the middle of the depth image shows the distance in mm to the target. 
 + 
 +There are 3 operating modes that determine the range of the system: 
 + 
 +  * Near - 25cm to 80cm 
 +  * Medium - 30cm to 4.5m 
 +  * Far - 3m to 6m 
 + 
 +When in a certain operating mode the system will measure distances outside of the mode's range but those will not be accurate.  
 + 
 +The evaluation application also displays the temperature in deg C of the camera (AFE) and laser boards as read from the temperature sensors installed on each board. 
 + 
 +The framerate at which data is acquired from the system is constantly updated on the GUI. The camera board outputs data at 30 frames per second (fps), but due to USB connection limitations,​ the host PC acquires the frames at a lower rate. 
 + 
 + 
 +==== Enabling the point cloud display in aditof-demo ==== 
 + 
 +  * The demo application has the capability to display a point cloud image if it detects an OpenCV module called viz. 
 +Unfortunately OpenCV does not provide binaries for this module so a manual build is needed. The steps required to  
 +install OpenCV and include it in the project are presented here: 
 +[[https://​github.com/​analogdevicesinc/​aditof_sdk/​blob/​master/​doc/​linux/​build_instructions.md#enabling-the-point-cloud-display-in-aditof-demo|Enable Point Cloud Aditof-Demo]] 
 + 
 +  * If aditof-demo finds all the OpenCV required modules a button in the interface will allow you to display the point cloudBy toggling the button a separate window will appear. 
 +{{ :resources:​eval:​user-guides:​ad-96tof1-ebz:​aditof_demo_pointCloud.png?​800 ​aditof-demo}}
  
resources/eval/user-guides/ad-96tof1-ebz/ug_xavier_nx.txt · Last modified: 17 Dec 2021 13:01 by Septimiu Vana