Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:eval:user-guides:ad-96tof1-ebz:calibration [11 Nov 2020 14:07]
Andrei Cozma [Introduction]
resources:eval:user-guides:ad-96tof1-ebz:calibration [03 Jan 2021 21:46]
Robin Getz fix links
Line 2: Line 2:
  
 ==== Introduction ==== ==== Introduction ====
-The [[https://​www.analog.com/​en/​design-center/​evaluation-hardware-and-software/​evaluation-boards-kits/​AD-96TOF1-EBZ.html|AD-96TOF1-EBZ]] is a pulsed Time-of-Flight (ToF) system. Is consists of a CCD sensor, an illumination source (VCSEL), and an analog front-end (AFE) with a ToF processor. To calculate depth a target scene is illuminated,​ the returned light is captured by the CCD sensor. The AFE reads the captured data and processes it to depth. In the current setup, there are 3 modes that can be programmed into the AFE to operate the camera at different ranges. Each mode operates on different firmware located in the config/​BM_Kit_RevC/​ or config/​BM_Kit_RevD/​ directory of the calibration folder. Depending on the board version, the folder from config/​BM_Kit_RevC or BM_Kit_RevD must be renamed to config/​BM_Kit before running the calibration software.+The [[adi>en/​design-center/​evaluation-hardware-and-software/​evaluation-boards-kits/​AD-96TOF1-EBZ.html|AD-96TOF1-EBZ]] is a pulsed Time-of-Flight (ToF) system. Is consists of a CCD sensor, an illumination source (VCSEL), and an analog front-end (AFE) with a ToF processor. To calculate depth a target scene is illuminated,​ the returned light is captured by the CCD sensor. The AFE reads the captured data and processes it to depth. In the current setup, there are 3 modes that can be programmed into the AFE to operate the camera at different ranges. Each mode operates on different firmware located in the config/​BM_Kit_RevC/​ or config/​BM_Kit_RevD/​ directory of the calibration folder. Depending on the board version, the folder from config/​BM_Kit_RevC or BM_Kit_RevD must be renamed to config/​BM_Kit before running the calibration software.
  
 ==== Calibration Overview ==== ==== Calibration Overview ====
resources/eval/user-guides/ad-96tof1-ebz/calibration.txt · Last modified: 03 Jan 2021 21:46 by Robin Getz