Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:eval:user-guide:adaq8092-eval-board [29 Jul 2022 06:22] Micheeko Loyolaresources:eval:user-guide:adaq8092-eval-board [30 Aug 2022 06:20] (current) Micheeko Loyola
Line 118: Line 118:
   * 1. Open the ACE software.   * 1. Open the ACE software.
   * 2. In the **Start** window, wait until the software recognizes the **"ADAQ8092 Board"** as an attached hardware, and then double-click on it to go to the "ADAQ8092 Board" window (refer to **Figure 9**).   * 2. In the **Start** window, wait until the software recognizes the **"ADAQ8092 Board"** as an attached hardware, and then double-click on it to go to the "ADAQ8092 Board" window (refer to **Figure 9**).
-{{ :resources:eval:user-guide:adaq8092:start_window.png?800 |}} +{{:resources:eval:user-guide:adaq8092:start_window_final.png?800|}}
 <WRAP centeralign>**//Figure 9. Start Window//** </WRAP> <WRAP centeralign>**//Figure 9. Start Window//** </WRAP>
     * 3. In the **ADAQ8092 Board** window, here you will see the simple block diagram of the evaluation board of the ADAQ8092, double-click the "ADAQ8092" icon from the block diagram to go to the "ADAQ8092" chip window (refer to **Figure 10**).     * 3. In the **ADAQ8092 Board** window, here you will see the simple block diagram of the evaluation board of the ADAQ8092, double-click the "ADAQ8092" icon from the block diagram to go to the "ADAQ8092" chip window (refer to **Figure 10**).
Line 125: Line 124:
 <WRAP centeralign>**//Figure 10. ADAQ8092 Board Window//** </WRAP> <WRAP centeralign>**//Figure 10. ADAQ8092 Board Window//** </WRAP>
   * 4. In the **ADAQ8092** chip window, click "Proceed to Analysis", to start the evaluation. //Note: Here you change the device attributes before starting the evaluation such as: alt_bit_pol_en , data_rand_en, dout_en, pd_gpio, pd_mode, sampling_frequency, test_mode, and twos_complement.//   * 4. In the **ADAQ8092** chip window, click "Proceed to Analysis", to start the evaluation. //Note: Here you change the device attributes before starting the evaluation such as: alt_bit_pol_en , data_rand_en, dout_en, pd_gpio, pd_mode, sampling_frequency, test_mode, and twos_complement.//
-{{ :resources:eval:user-guide:adaq8092:chip_image_final.png?800 |}}+{{:resources:eval:user-guide:adaq8092:chip_image_final2.png?800|}}
 <WRAP centeralign>**//Figure 11. ADAQ8092 (Chip) Window//** </WRAP> <WRAP centeralign>**//Figure 11. ADAQ8092 (Chip) Window//** </WRAP>
  
resources/eval/user-guide/adaq8092-eval-board.txt · Last modified: 30 Aug 2022 06:20 by Micheeko Loyola