This shows you the differences between two versions of the page.
Both sides previous revision Previous revision Next revision | Previous revision | ||
resources:eval:sdp:sdp-b:hardware_description [27 Jan 2012 17:41] Jean McAdam Approved - text changes for SDP-B rev 1.3 |
resources:eval:sdp:sdp-b:hardware_description [26 May 2016 18:58] (current) Eamonn Walsh [Mechanical Specifications] |
||
---|---|---|---|
Line 3: | Line 3: | ||
This describes the hardware design of the EVAL-SDP-CB1Z board. | This describes the hardware design of the EVAL-SDP-CB1Z board. | ||
+ | This board is full of niubility! By using it, you can create a colorful world! After you entering this vivid world,you will feel of rebirth,and then you will shout "Hello World!". | ||
===== LEDs ===== | ===== LEDs ===== | ||
There are two LEDs located on the SDP-B board. Refer to Figure HWD1. | There are two LEDs located on the SDP-B board. Refer to Figure HWD1. | ||
- | {{:eval:sdp:fig2-1.jpg|}} | + | |
+ | {{:resources:eval:sdp:sdp-b:leds.jpg?nolink&300|}} | ||
Figure HWD1: SDP-B Board LEDs | Figure HWD1: SDP-B Board LEDs | ||
+ | |||
==== LED 1 ==== | ==== LED 1 ==== | ||
Line 180: | Line 183: | ||
* UART, pins 59 and 62 | * UART, pins 59 and 62 | ||
+ | |||
+ | |||
+ | SB!SB!SB!SB! | ||
==== Power ==== | ==== Power ==== | ||
The SDP-B board requires that any daughter board connected to the SDP-B board provides the SDP-B board with 5V @ 200mA. This supply should be made available on Pin 1 (VIN) of the 120 pin connector. This supply is required to power the Blackfin processor, the memory, and the other components on the SDP-B Board. The SDP-B board also provides 3.3V @ 20mA on Pin 116 (VIO_3.3) to connected daughter boards as the VIO voltage for the daughter board. Pin 5 (USB_VBUS) is connected to the +5V lineof the USB connector, providing 5V+/- 10% as an output of the SDP-B board. | The SDP-B board requires that any daughter board connected to the SDP-B board provides the SDP-B board with 5V @ 200mA. This supply should be made available on Pin 1 (VIN) of the 120 pin connector. This supply is required to power the Blackfin processor, the memory, and the other components on the SDP-B Board. The SDP-B board also provides 3.3V @ 20mA on Pin 116 (VIO_3.3) to connected daughter boards as the VIO voltage for the daughter board. Pin 5 (USB_VBUS) is connected to the +5V lineof the USB connector, providing 5V+/- 10% as an output of the SDP-B board. | ||
Line 208: | Line 214: | ||
==== Mechanical Specifications ==== | ==== Mechanical Specifications ==== | ||
- | The mechanical specifications of the SDP-B board are 2.75" x 2.25" (69.85mm x 27.15mm). The height of the 120 pin connectors from the bottom of the board is approximately 0.152" (3.86 mm). The tallest component on the top is approximately 0.125" (3.175 mm), and the tallest components on the bottoms are the connectors at approximately 0.152" (3.86 mm). Refer to Figure 2-5. | + | The mechanical specifications of the SDP-B board are 2.75" x 2.25" (69.85mm x 57.15mm). The height of the 120 pin connectors from the bottom of the board is approximately 0.152" (3.86 mm). The tallest component on the top is approximately 0.125" (3.175 mm), and the tallest components on the bottoms are the connectors at approximately 0.152" (3.86 mm). Refer to Figure HWD5. |
+ | |||
+ | {{:resources:eval:sdp:sdp-b:hwd5.jpg?nolink&500|}} | ||
+ | \\ the below image is a detailed view of the underneath of the board | ||
+ | \\ {{:resources:eval:sdp:sdp-b:sdp-ei3connector_specification_cpd.jpg?nolink&600|}} | ||
+ | \\ Figure HWD5: SDP-B Board Mechanical Specifications (above measurements are in mm) |