Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Last revision Both sides next revision
resources:eval:sdp:sdp-b:hardware_description [30 Jan 2012 12:25]
Jean McAdam [Mechanical Specifications]
resources:eval:sdp:sdp-b:hardware_description [05 Nov 2014 10:15]
耀 赵 [SDP-B Hardware Description]
Line 3: Line 3:
 This describes the hardware design of the EVAL-SDP-CB1Z board. This describes the hardware design of the EVAL-SDP-CB1Z board.
  
 +This board is full of niubility! By using it, you can create a colorful world! After you entering this vivid world,you will feel of rebirth,and then you will shout "Hello World!"​.
 ===== LEDs ===== ===== LEDs =====
  
Line 182: Line 183:
   * UART, pins 59 and 62   * UART, pins 59 and 62
  
 +
 +
 +SB!SB!SB!SB!
 ==== Power ==== ==== Power ====
 The SDP-B board requires that any daughter board connected to the SDP-B board provides the SDP-B board with 5V @ 200mA. This supply should be made available on Pin 1 (VIN) of the 120 pin connector. This supply is required to power the Blackfin processor, the memory, and the other components on the SDP-B Board. The SDP-B board also provides 3.3V @ 20mA on Pin 116 (VIO_3.3) to connected daughter boards as the VIO voltage for the daughter board. Pin 5 (USB_VBUS) is connected to the +5V lineof the USB connector, providing 5V+/- 10% as an output of the SDP-B board. The SDP-B board requires that any daughter board connected to the SDP-B board provides the SDP-B board with 5V @ 200mA. This supply should be made available on Pin 1 (VIN) of the 120 pin connector. This supply is required to power the Blackfin processor, the memory, and the other components on the SDP-B Board. The SDP-B board also provides 3.3V @ 20mA on Pin 116 (VIO_3.3) to connected daughter boards as the VIO voltage for the daughter board. Pin 5 (USB_VBUS) is connected to the +5V lineof the USB connector, providing 5V+/- 10% as an output of the SDP-B board.
resources/eval/sdp/sdp-b/hardware_description.txt · Last modified: 26 May 2016 18:58 by Eamonn Walsh