This chapter provides specific information to assist you with using the SDP board as part of your evaluation system.
Your EVAL-SDP-CB1Z board package contains the following items.
Contact the vendor where you purchased your SDP board or contact Analog Devices, Inc. if any item is missing.
For correct operation of the SDP board, your computer must have the following minimum configuration
The SDP board evaluation system contains ESD (electrostatic discharge) sensitive devices. Electrostatic charges readily accumulate on the human body and equipment and can discharge without detection. Permanent damage may occur on devices subjected to high-energy discharges. Proper ESD precautions are recommended to avoid performance degradation or loss of functionality. Store unused SDP boards in the protective shipping package.
When removing the SDP board from the package, handle the board carefully to avoid the discharge of static electricity, which can damage some components.
Perform the following tasks to safely install the SDP board onto the computer.
There are two stages in the software application installation procedure. The first installs the application software. The second installs the .NET Framework 3.5 and the necessary drivers.
Before using the SDP board, verify the driver software has installed properly.
Figure GS1 : Device Manager showing correct SDP installation
The following sections describe how to safely power up and down the SDP.