Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:eval:sdp:eval-adrf6755 [01 Mar 2022 16:30] – [Accessing ACE Software:] Shine Cabatanresources:eval:sdp:eval-adrf6755 [06 Apr 2023 10:42] (current) – [Accessing ACE Software:] Gokhan Karaova
Line 12: Line 12:
  
 [[ACE - Getting Started [Analog Devices Wiki]]] [[ACE - Getting Started [Analog Devices Wiki]]]
- 
-{{ :resources:eval:sdp:board.adrf6755.1.2021.45400-dev0012.zip | Dev Release}} 
 ===== Downloading the ADRF6755 Plugin from ACE:===== ===== Downloading the ADRF6755 Plugin from ACE:=====
  
Line 20: Line 18:
 To download the ACE plugin for the ADRF6755 evaluation board, first open up the ACE software on your computer as seen below: To download the ACE plugin for the ADRF6755 evaluation board, first open up the ACE software on your computer as seen below:
  
-{{ :resources:eval:sdp:acemain.png?600 |}}+{{ :resources:eval:sdp:adrf6755_ace_mainmenu.png |}}
  
 Upon opening ACE, navigate to the "Available Packages" section in the "Plug-in Manager" tab as seen below: Upon opening ACE, navigate to the "Available Packages" section in the "Plug-in Manager" tab as seen below:
  
-{{ :resources:eval:sdp:aceplugin.png?600 |}}+{{ :resources:eval:sdp:adrf6755_ace_pluginmanager_2.png |}}
  
 Once you have navigated to this section of the ACE software, inspect the contents in the center of the screen until you locate the item labeled "Board.ADRF6755". Once you have navigated to this section of the ACE software, inspect the contents in the center of the screen until you locate the item labeled "Board.ADRF6755".
Line 40: Line 38:
 Once the hardware setup has been completed navigate to the ACE start menu as seen below and look for the board to connect to through ACE in the "Attached Hardware" section. If the option to connect doesn't show up immediately wait and try pressing the refresh button. Once the hardware setup has been completed navigate to the ACE start menu as seen below and look for the board to connect to through ACE in the "Attached Hardware" section. If the option to connect doesn't show up immediately wait and try pressing the refresh button.
  
-{{ :resources:eval:sdp:acestart.png?600 |}}+{{ :resources:eval:sdp:adrf6755_ace_mainmenu.png |}}
  
 Once the plugin opens it should look something like the image below: Once the plugin opens it should look something like the image below:
  
-{{ :resources:eval:sdp:ace6755.png?600 |}}+{{ :resources:eval:sdp:adrf6755_ace_pluginview.png |}}
  
 ===== Performing Actions With the ADRF6755 ACE GUI ===== ===== Performing Actions With the ADRF6755 ACE GUI =====
- 
-{{ :resources:eval:sdp:6755gui.png?600 |}} 
  
 ==== Initialize LO Frequency ==== ==== Initialize LO Frequency ====
resources/eval/sdp/eval-adrf6755.txt · Last modified: 06 Apr 2023 10:42 by Gokhan Karaova