Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:eval:sdp:eval-adrf6755 [09 Aug 2021 15:50]
Eric Webb
resources:eval:sdp:eval-adrf6755 [09 Aug 2021 16:20]
Eric Webb
Line 78: Line 78:
  
 This section is used to enable/​disable the lock detector as well as determine its pulse count and precision ​ This section is used to enable/​disable the lock detector as well as determine its pulse count and precision ​
 +
 +===== Basic Test Case =====
 +
 +1. Begin by enabling the modulator power up setting ​
 +
 +2. Attach a +5.0V supply to the DUT pin with a current limit of 400mA
 +
 +3. Attach a Spectrum Analyzer to the RFOut pin of the ADRF6755
 +
 +4. Hit the apply button at the bottom of the ACE 
 +
 +5. Set the center frequency of the Spectrum Analyzer to 1875MHz and the span to 80MHz
 +
 +{{:​resources:​eval:​sdp:​adrf6755testcase.jpg?​400|}}
 +
 +6. Measure the output frequency and output power of the main RF output on the spectrum analyzer. The highest power tone at 1850MHz should read be greater than -4dBm
 +
 +7. The power of the carrier feedthrough at 1875MHz should be at least 45dB below the 1850MHz tone (-45dBc)
 +
 +8. The power of the suppressed sideband at 1900MHz should be at least 30dB below the 1850MHz tone (-30dBc)
  
resources/eval/sdp/eval-adrf6755.txt · Last modified: 09 Aug 2021 16:20 by Eric Webb