This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | |||
resources:eval:hmcad15xx [06 Feb 2023 06:29] Deferson Romero Draft 2/6 |
resources:eval:hmcad15xx [09 Feb 2023 07:41] Deferson Romero |
||
---|---|---|---|
Line 81: | Line 81: | ||
- For [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-HMCAD1511.html|HMCAD1511-EBZ]], connect another continuous wave generator as the ADC clock. Set the clock frequency to **1GHz** and **10dBm** output level. | - For [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-HMCAD1511.html|HMCAD1511-EBZ]], connect another continuous wave generator as the ADC clock. Set the clock frequency to **1GHz** and **10dBm** output level. | ||
- Going back to ACE Software, click **Proceed to Analysis** button and click on the **FFT** tab. Click **Run Once** button under **Capture** wizard to capture an FFT plot. | - Going back to ACE Software, click **Proceed to Analysis** button and click on the **FFT** tab. Click **Run Once** button under **Capture** wizard to capture an FFT plot. | ||
- | - Observe the fundamental frequency and power. Adjust the signal source unti; obtain approximately -1dBFS fundamental power at 70MHz.<WRAP centeralign>{{ :resources:eval:hmcad1511_fundpower_-1dbfs.jpg?400 |}}//Figure 4. HMCAD1511-EBZ Fundamental Frequency and Power//</WRAP> | + | - Observe the fundamental frequency and power. Adjust the signal source until fundamental power obtains approximately -1dBFS at 70MHz.<WRAP centeralign>{{ :resources:eval:hmcad1511_fundpower_-1dbfs.jpg?400 |}}//Figure 4. HMCAD1511-EBZ Fundamental Frequency and Power//</WRAP> |
- If fundamental power achieved, click **Zoom to Fit** ({{:resources:eval:hmcad1511_zoomtofit.jpg}}) to show graph at Fs/2, then click **Show Annotations** ({{:resources:eval:hmcad1511_annotations.jpg}}) to show all the spurs' annotation within the plot. Refer to Figure 5.<WRAP centeralign>{{ :resources:eval:hmcad-8bit-1g-70m-single-fft.jpg?900 |}}//Figure 5. HMCAD1511-EBZ (8-bit, single channel, Fs=1GHz, Fin=70MHz) FFT Analysis Results//</WRAP> | - If fundamental power achieved, click **Zoom to Fit** ({{:resources:eval:hmcad1511_zoomtofit.jpg}}) to show graph at Fs/2, then click **Show Annotations** ({{:resources:eval:hmcad1511_annotations.jpg}}) to show all the spurs' annotation within the plot. Refer to Figure 5.<WRAP centeralign>{{ :resources:eval:hmcad-8bit-1g-70m-single-fft.jpg?900 |}}//Figure 5. HMCAD1511-EBZ (8-bit, single channel, Fs=1GHz, Fin=70MHz) FFT Analysis Results//</WRAP> | ||
- To save the **Data Set**, click **Export** button on the **Results** wizard. Also, you click **Import** button to review the saved data set with a file format of "//.acesamples//".<WRAP centeralign>{{ :resources:eval:hmcad-result-table.jpg?400 |}}//Table 3. HMCAD1511-EBZ (8-bit, single channel, Fs=1GHz, Fin=70MHz) Results Comparison.//</WRAP> | - To save the **Data Set**, click **Export** button on the **Results** wizard. Also, you click **Import** button to review the saved data set with a file format of "//.acesamples//".<WRAP centeralign>{{ :resources:eval:hmcad-result-table.jpg?400 |}}//Table 3. HMCAD1511-EBZ (8-bit, single channel, Fs=1GHz, Fin=70MHz) Results Comparison.//</WRAP> |