This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:ezlinx:windows_xp_installation_and_setup_guide [20 Aug 2013 12:10] – [Setting up the ezLINX board IP address] Liam Delahunt | resources:eval:ezlinx:windows_xp_installation_and_setup_guide [03 Jan 2021 22:04] (current) – fix links Robin Getz | ||
---|---|---|---|
Line 21: | Line 21: | ||
Install the ezLINX PC Application setup found in the Software/PC Application Installation folder located on the ezLINX Software Package DVD. The latest version of this software can be downloaded from the link below. \\ | Install the ezLINX PC Application setup found in the Software/PC Application Installation folder located on the ezLINX Software Package DVD. The latest version of this software can be downloaded from the link below. \\ | ||
<WRAP center round download 60%> | <WRAP center round download 60%> | ||
- | [[http:// | + | [[adi>static/ |
</ | </ | ||
Run the setup by double clicking on the setup.exe file. This should start the installation process and when completed the window below will open: | Run the setup by double clicking on the setup.exe file. This should start the installation process and when completed the window below will open: | ||
Line 32: | Line 32: | ||
===== Installing the USB drivers ===== | ===== Installing the USB drivers ===== | ||
<WRAP center round download 60%> | <WRAP center round download 60%> | ||
- | [[http:// | + | [[adi>static/ |
</ | </ | ||