Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:ezlinx:usb-ip-config [28 Jun 2012 13:13] – Added addtitional instructions Matthew Hutchinson | resources:eval:ezlinx:usb-ip-config [14 Apr 2021 23:34] (current) – added retired page tag Neil Quinn |
---|
| {{page>/wiki/common#retired&nofooter&noheader}} |
| |
\\ | \\ |
[[resources/eval/ezlinx|ezLINX™ iCoupler® Isolated Interface Development Environment Homepage]] | [[resources/eval/ezlinx|ezLINX™ iCoupler® Isolated Interface Development Environment Homepage]] |
| |
The device can also be found by accessing the device manager (Control Panel -> System -> Hardware) and looking for the Linux USB Ethernet/RNDIS Gadget under Network Adapters. Right click on the Linux USB Ethernet/RNDIS Gadget and select "update driver". | The device can also be found by accessing the device manager (Control Panel -> System -> Hardware) and looking for the Linux USB Ethernet/RNDIS Gadget under Network Adapters. Right click on the Linux USB Ethernet/RNDIS Gadget and select "update driver". |
| |
| {{:resources:eval:ezlinx:accessingsystemsweb.png?500x400| }} |
| {{ :resources:eval:ezlinx:accessingdevicemanagerweb.png?400x400|}} \\ \\ \\ |
| {{ :resources:eval:ezlinx:locatingusbgadgetweb.png?600x400 |Figure 4. Locating USB Gadget }} |
| |
| \\ \\ |
| |
Click on the pop-up which brings up the "Found New Hardware" dialog, select "Install from a list or specific location (Advanced)". Next select "Don't Search, I will choose the driver to install". Alternatively the driver can also be installed by selecting the "Search for the best driver in these locations", ticking the box marked "include this location in the search" and then selecting the folder which contains the extracted contents of the USB Gadget Driver File. | Click on the pop-up which brings up the "Found New Hardware" dialog, select "Install from a list or specific location (Advanced)". Next select "Don't Search, I will choose the driver to install". Alternatively the driver can also be installed by selecting the "Search for the best driver in these locations", ticking the box marked "include this location in the search" and then selecting the folder which contains the extracted contents of the USB Gadget Driver File. |
| |
| |
Once the USB driver is sucessfully installed, the IP address for the device must be configured. | Once the USB driver is sucessfully installed, the IP address for the device must be configur |
| ed. |
| |
===== Network Adapter IP Configuration ===== | ===== Network Adapter IP Configuration ===== |