This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
ezlinx:isolated-usb [10 May 2012 10:57] – Added board to board communications section Neil Quinn | resources:eval:ezlinx:isolated-usb [03 Jan 2021 22:04] (current) – fix links Robin Getz | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== Isolated USB ====== | ||
- | |||
- | ===== Hardware Implementation ===== | ||
- | |||
- | The Isolated USB port is implemented using the [[http:// | ||
- | |||
- | |||
- | |||
- | |||
- | {{ : | ||
- | |||
\\ | \\ | ||
- | + | [[resources/eval/ezlinx|ezLINX™ iCoupler® Isolated Interface Development Environment Homepage]] | |
- | The VBUS1 and VDD1 of the [[http://www.analog.com/ | + | |
\\ | \\ | ||
+ | ====== ezLINX™ Isolated USB Implementation====== | ||
- | ===== Setup ===== | + | ===== Hardware Implementation |
- | ==== Device Installation ==== | + | The Isolated USB port is implemented using the [[adi> |
- | A driver must be installed in order to connect to the //ez//LINX Development Platform using the sample PC Application. Instructions to install this device driver are given below. | ||
- | <WRAP center round download 20% right> | ||
- | {{: | ||
- | </ | ||
- | <WRAP center round important 62% left> | ||
- | **Warning: | ||
- | </ | ||
- | \\ | ||
- | |||
- | First download and extract the above USB Gadget Driver file. To install the USB gadget plug it into the target PC. A pop-up will appear (see below) saying that Windows has found a new hardware device called a " | ||
- | |||
- | {{ : | ||
- | |||
- | Click on the pop-up which brings up the "Found New Hardware" | ||
- | |||
- | {{: | ||
- | {{ : | ||
- | |||
- | \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ | ||
- | |||
- | If a " | ||
+ | {{ : | ||
\\ | \\ | ||
- | {{: | + | The VBUS1 and VDD1 of the [[adi> |
- | {{ : | + | |
- | + | ||
- | \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ | + | |
- | + | ||
- | + | ||
- | Once the USB driver | + | |
- | + | ||
- | ==== IP Configuration ==== | + | |
- | + | ||
- | To set up the network adapter to connect with the // | + | |
- | \\ | + | |
- | + | ||
- | {{ : | + | |
\\ | \\ | ||
- | The below window should then open. Select "Use the following IP address" | ||
- | |||
- | **IP Address:** 192.168.1.100\\ | ||
- | **Subnet mask:** 255.255.255.0\\ | ||
- | **Default gateway:** 192.168.1.1\\ | ||
- | \\ | ||
- | {{ : | ||
- | \\ | ||
- | |||
- | Select Ok to confirm. Now the host and the device are on the same network. | ||
- | |||
- | <WRAP center round important 60%> | ||
- | **Note:** Switching the USB port used for the Gadget Ethernet device will require you to perform the above steps again, setting up the appropriate IP address and gateway for the USB device. | ||
- | </ | ||
- | |||
- | **Note:** When connecting two //ez//LINX Development Platforms to the same P.C. for board to board communication, | ||
- | |||
- | |||
- | **Example Configuration: | ||
- | \\ \\ | ||
- | **// | ||
- | **IP Address:** 192.168.1.21\\ | ||
- | **Subnet Mask:** 255.255.255.0\\ | ||
- | **Default Gateway:** 192.168.1.1\\ | ||
- | |||
- | \\ | ||
- | |||
- | **Isolated USB Network Adapter 1:**\\ | ||
- | **IP Address: | ||
- | **Subnet Mask: | ||
- | **Default Gateway:** 192.168.1.1 | ||
- | |||
- | \\ | ||
- | |||
- | **// | ||
- | **IP Address:** 192.168.2.21\\ | ||
- | **Subnet Mask:** 255.255.255.0\\ | ||
- | **Default Gateway:** 192.168.2.1 | ||
- | |||
- | \\ | ||
- | |||
- | **Isolated USB Network Adapter 2:**\\ | ||
- | **IP Address:** 192.168.2.100\\ | ||
- | **Subnet Mask:** 255.255.255.0\\ | ||
- | **Default Gateway:** 192.168.2.1\\ | ||
- | |||
- | \\ |