This shows you the differences between two versions of the page.
Both sides previous revision Previous revision Next revision | Previous revision | ||
resources:eval:ezlinx:isolated-usb [16 May 2012 18:50] Hein Marais Approved |
resources:eval:ezlinx:isolated-usb [03 Jan 2021 22:04] Robin Getz fix links |
||
---|---|---|---|
Line 1: | Line 1: | ||
\\ | \\ | ||
- | [[resources/eval/ezlinx|ezLINX™ iCoupler® Isolated Interface Development Platform Homepage]] | + | [[resources/eval/ezlinx|ezLINX™ iCoupler® Isolated Interface Development Environment Homepage]] |
\\ | \\ | ||
Line 7: | Line 7: | ||
===== Hardware Implementation ===== | ===== Hardware Implementation ===== | ||
- | The Isolated USB port is implemented using the [[http://www.analog.com/adum3160|ADuM3160]] Full speed USB Isolator. The [[http://www.analog.com/adum3160|ADuM3160]] connects to the integrated USB PHY of the ADSP-BF548 and is capable of functioning at data rates of up to 12Mbit/s. Figure 1 below shows a circuit diagram of the implementation of the [[http://www.analog.com/adum3160|ADuM3160]] on the //ez//LINX hardware. | + | The Isolated USB port is implemented using the [[adi>adum3160|ADuM3160]] Full speed USB Isolator. The [[adi>adum3160|ADuM3160]] connects to the integrated USB PHY of the ADSP-BF548 and is capable of functioning at data rates of up to 12Mbit/s. Figure 1 below shows a circuit diagram of the implementation of the [[adi>adum3160|ADuM3160]] on the //ez//LINX hardware. |
Line 15: | Line 15: | ||
\\ | \\ | ||
- | The VBUS1 and VDD1 of the [[http://www.analog.com/adum3160|ADuM3160]] is powered from the 5V bus power supply. VBUS2 and VDD2 is powered from 3.3V generated by the //ez//LINX power supply. A mini USB-B connector is used for easy connection to a USB master. | + | The VBUS1 and VDD1 of the [[adi>adum3160|ADuM3160]] is powered from the 5V bus power supply. VBUS2 and VDD2 is powered from 3.3V generated by the //ez//LINX power supply. A mini USB-B connector is used for easy connection to a USB master. |
\\ | \\ | ||