Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:eval:ezlinx:isolated-spi [15 May 2012 16:15] – updated ezlinx link Andy Roseresources:eval:ezlinx:isolated-spi [03 Jan 2021 22:04] (current) – fix links Robin Getz
Line 1: Line 1:
 \\ \\
-[[resources/eval/ezlinx|ezLINX™ iCoupler® Isolated Interface Development Platform Homepage]]+[[resources/eval/ezlinx|ezLINX™ iCoupler® Isolated Interface Development Environment Homepage]]
 \\ \\
 ====== ezLINX™ Isolated SPI Implementation====== ====== ezLINX™ Isolated SPI Implementation======
  
-Two Isolated SPI ports are implemented using the [[http://www.analog.com/adum3401|ADuM3401]] and the [[http://www.analog.com/adum3402|ADuM3402]] //i//Coupler signal isolators and the [[http://www.analog.com/adum5000|ADuM5000]] //iso//Power Isolated DC to DC converter. The [[http://www.analog.com/adum3401|ADuM3401]] of the isolated SPI1 is connected to SPI0 of the ADSP-BF548. The [[http://www.analog.com/adum3402|ADuM3402]] is used for isolating the SPI slave select lines. Figure 1 below shows a circuit diagram of the implementation of Isolated SPI1 using the [[http://www.analog.com/adum3401|ADuM3401]], [[http://www.analog.com/adum3402|ADuM3402]], and [[http://www.analog.com/adum5000|ADuM5000]] on the //ez//LINX hardware.+Two Isolated SPI ports are implemented using the [[adi>adum3401|ADuM3401]] and the [[adi>adum3402|ADuM3402]] //i//Coupler signal isolators and the [[adi>adum5000|ADuM5000]] //iso//Power Isolated DC to DC converter. The [[adi>adum3401|ADuM3401]] of the isolated SPI1 is connected to SPI0 of the ADSP-BF548. The [[adi>adum3402|ADuM3402]] is used for isolating the SPI slave select lines. Figure 1 below shows a circuit diagram of the implementation of Isolated SPI1 using the [[adi>adum3401|ADuM3401]], [[adi>adum3402|ADuM3402]], and [[adi>adum5000|ADuM5000]] on the //ez//LINX hardware.
  
 {{ :ezlinx:isolatedspi1.png?nolink&900 |Figure 1. Isolated SPI1 schematic}} {{ :ezlinx:isolatedspi1.png?nolink&900 |Figure 1. Isolated SPI1 schematic}}
  
-To connect Isolated SPI1 as a master, connect jumpers JP5, JP7, JP9, JP11, JP13 and JP15 while leaving jumpers JP6, JP8, JP10, JP12, JP14 and JP16 open. To connect Isolated SPI1 as a slave, connect jumpers JP6, JP8, JP10, JP12, JP14 and JP16 while leaving jumpers JP5, JP7, JP9, JP11, JP13 and JP15 open. When connecting SPI1 as a slave JP20 should also be connectedenabling the slave select and serial clock inputs on the [[http://www.analog.com/adum3402|ADuM3402]].+To connect Isolated SPI1 as a master, connect jumpers JP5, JP7, JP9, JP11, JP13JP15, JP21 and JP36 while leaving jumpers JP6, JP8, JP10, JP12, JP14JP16, JP20 and JP37 open. To connect Isolated SPI1 as a slave, connect jumpers JP6, JP8, JP10, JP12, JP14JP16, JP20 and JP37 while leaving jumpers JP5, JP7, JP9, JP11, JP13JP15, JP21 and JP36 open. When connecting SPI1 as a slave, connecting JP20 enables the slave select and serial clock inputs on the [[adi>adum3402|ADuM3402]].
  
 These jumper settings are given in the table below: These jumper settings are given in the table below:
  
-|              ^  JP5  ^  JP6  ^  JP7  ^  JP8  ^  JP9  ^  JP10  ^  JP11  ^  JP12  ^  JP13  ^  JP14  ^  JP15  ^  JP16  ^  JP20  ^  JP21  ^ +|              ^  JP5  ^  JP6  ^  JP7  ^  JP8  ^  JP9  ^  JP10  ^  JP11  ^  JP12  ^  JP13  ^  JP14  ^  JP15  ^  JP16  ^  JP20  ^  JP21   JP36  ^  JP37  ^ 
-^  SPI1 Master  |  Connect  |  Open  |  Connect  |  Open  |  Connect  |  Open  |  Connect  |  Open  |  Connect  |  Open  |  Connect  |  Open  |  Open  |  Connect / Floating  | +^  SPI1 Master  |  Connect  |  Open  |  Connect  |  Open  |  Connect  |  Open  |  Connect  |  Open  |  Connect  |  Open  |  Connect  |  Open  |  Open  |  Connect |  Connect  |  Open  |  
-^  SPI1 Slave  |  Open  |  Connect  |  Open  |  Connect  |  Open  |  Connect  |  Open  |  Connect  |  Open  |  Connect  |  Open  |  Connect  |  Connect  |  Open  |+^  SPI1 Slave  |  Open  |  Connect  |  Open  |  Connect  |  Open  |  Connect  |  Open  |  Connect  |  Open  |  Connect  |  Open  |  Connect  |  Connect  |  Open   Open  |  Connect  |
  
 \\ \\
  
  
-The [[http://www.analog.com/adum3401|ADuM3401]] of the isolated SPI2 is connected to SPI2 of the ADSP-BF548. The [[http://www.analog.com/adum3402|ADuM3402]] is used for isolating the SPI slave select lines. Figure 2 below shows a circuit diagram of the implementation of Isolated SPI2 using the [[http://www.analog.com/adum3401|ADuM3401]], [[http://www.analog.com/adum3402|ADuM3402]] and [[http://www.analog.com/adum5000|ADuM5000]] on the //ez//LINX hardware.+The [[adi>adum3401|ADuM3401]] of the isolated SPI2 is connected to SPI2 of the ADSP-BF548. The [[adi>adum3402|ADuM3402]] is used for isolating the SPI slave select lines. Figure 2 below shows a circuit diagram of the implementation of Isolated SPI2 using the [[adi>adum3401|ADuM3401]], [[adi>adum3402|ADuM3402]] and [[adi>adum5000|ADuM5000]] on the //ez//LINX hardware.
  
 {{ :ezlinx:isolatedspi2.png?nolink&900 |Figure 2. Isolated SPI2 schematic}} {{ :ezlinx:isolatedspi2.png?nolink&900 |Figure 2. Isolated SPI2 schematic}}
  
-To connect Isolated SPI2 as a master, connect jumpers JP22, JP24, JP26, JP28, JP30 and JP32 while leaving jumpers JP23, JP25, JP27, JP29, JP31 and JP33 open. To connect Isolated SPI2 as a slave, connect jumpers JP23, JP25, JP27, JP29, JP31 and JP33 while leaving jumpers JP22, JP24, JP26, JP28, JP30 and JP32 open. When connecting SPI2 as a slave JP34 should also be connected, enabling the slave select and serial clock inputs on the [[http://www.analog.com/adum3402|ADuM3402]].+To connect Isolated SPI2 as a master, connect jumpers JP22, JP24, JP26, JP28, JP30JP32, JP35 and JP38 while leaving jumpers JP23, JP25, JP27, JP29, JP31JP33, JP34 and JP39 open. To connect Isolated SPI2 as a slave, connect jumpers JP23, JP25, JP27, JP29, JP31JP33, JP34 and JP39 while leaving jumpers JP22, JP24, JP26, JP28, JP30JP32, JP35 and JP38 open. When connecting SPI2 as a slave JP34 should also be connected, enabling the slave select and serial clock inputs on the [[adi>adum3402|ADuM3402]].
  
  
 These jumper settings are given in the table below: These jumper settings are given in the table below:
  
-|              ^  JP22  ^  JP23  ^  JP24  ^  JP25  ^  JP26  ^  JP27  ^  JP28  ^  JP29  ^  JP30  ^  JP31  ^  JP32  ^  JP33  ^  JP34  ^  JP35  ^ +|              ^  JP22  ^  JP23  ^  JP24  ^  JP25  ^  JP26  ^  JP27  ^  JP28  ^  JP29  ^  JP30  ^  JP31  ^  JP32  ^  JP33  ^  JP34  ^  JP35   JP38  ^  JP39  ^ 
-^  SPI2 Master  |  Connect  |  Open  |  Connect  |  Open  |  Connect  |  Open  |  Connect  |  Open  |  Connect  |  Open  |  Connect  |  Open  |  Open  |  Connect / Floating  | +^  SPI2 Master  |  Connect  |  Open  |  Connect  |  Open  |  Connect  |  Open  |  Connect  |  Open  |  Connect  |  Open  |  Connect  |  Open  |  Open  |  Connect |  Connect  |  Open  | 
-^  SPI2 Slave  |  Open  |  Connect  |  Open  |  Connect  |  Open  |  Connect  |  Open  |  Connect  |  Open  |  Connect  |  Open  |  Connect  |  Connect  |  Open  |+^  SPI2 Slave  |  Open  |  Connect  |  Open  |  Connect  |  Open  |  Connect  |  Open  |  Connect  |  Open  |  Connect  |  Open  |  Connect  |  Connect  |  Open   Open  |  Connect  |
  
 \\ \\
  
-VDD1 of the [[http://www.analog.com/adum3401|ADuM3401]], [[http://www.analog.com/adum3402|ADuM3402]] and VDD1 of the [[http://www.analog.com/adum5000|ADuM5000]] are powered by 3.3V. The [[http://www.analog.com/adum5000|ADuM5000]] will generate an isolated 3.3V and is used to supply power to VDD2 of the [[http://www.analog.com/adum3401|ADuM3401]] and [[http://www.analog.com/adum3402|ADuM3402]].+VDD1 of the [[adi>adum3401|ADuM3401]], [[adi>adum3402|ADuM3402]] and VDD1 of the [[adi>adum5000|ADuM5000]] are powered by 3.3V. The [[adi>adum5000|ADuM5000]] will generate an isolated 3.3V and is used to supply power to VDD2 of the [[adi>adum3401|ADuM3401]] and [[adi>adum3402|ADuM3402]].
  
 Two seven pin screw terminal connectors, J10 and J25 are used for easy access to the SPISCK (Pin 1), SPIMOSI (Pin 2), SPISEL1/SPISS (Pin 3), SPIMISO (Pin 4). SPISEL2 (Pin 5), SPISEL3 (Pin 6) and SPI_ISO_GND (Pin 7). Two seven pin screw terminal connectors, J10 and J25 are used for easy access to the SPISCK (Pin 1), SPIMOSI (Pin 2), SPISEL1/SPISS (Pin 3), SPIMISO (Pin 4). SPISEL2 (Pin 5), SPISEL3 (Pin 6) and SPI_ISO_GND (Pin 7).
  
  
resources/eval/ezlinx/isolated-spi.1337091310.txt.gz · Last modified: 15 May 2012 16:15 by Andy Rose