Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
Last revision Both sides next revision
resources:eval:ezlinx:isolated-spi [16 May 2012 18:53]
Hein Marais Approved
resources:eval:ezlinx:isolated-spi [23 Jul 2012 14:58]
Hein Marais Approved
Line 1: Line 1:
 \\ \\
-[[resources/​eval/​ezlinx|ezLINX™ iCoupler® Isolated Interface Development ​Platform ​Homepage]]+[[resources/​eval/​ezlinx|ezLINX™ iCoupler® Isolated Interface Development ​Environment ​Homepage]]
 \\ \\
 ====== ezLINX™ Isolated SPI Implementation====== ====== ezLINX™ Isolated SPI Implementation======
Line 8: Line 8:
 {{ :​ezlinx:​isolatedspi1.png?​nolink&​900 |Figure 1. Isolated SPI1 schematic}} {{ :​ezlinx:​isolatedspi1.png?​nolink&​900 |Figure 1. Isolated SPI1 schematic}}
  
-To connect Isolated SPI1 as a master, connect jumpers JP5, JP7, JP9, JP11, JP13 and JP15 while leaving jumpers JP6, JP8, JP10, JP12, JP14 and JP16 open. To connect Isolated SPI1 as a slave, connect jumpers JP6, JP8, JP10, JP12, JP14 and JP16 while leaving jumpers JP5, JP7, JP9, JP11, JP13 and JP15 open. When connecting SPI1 as a slave JP20 should also be connectedenabling ​the slave select and serial clock inputs on the [[http://​www.analog.com/​adum3402|ADuM3402]].+To connect Isolated SPI1 as a master, connect jumpers JP5, JP7, JP9, JP11, JP13JP15, JP21 and JP36 while leaving jumpers JP6, JP8, JP10, JP12, JP14JP16, JP20 and JP37 open. To connect Isolated SPI1 as a slave, connect jumpers JP6, JP8, JP10, JP12, JP14JP16, JP20 and JP37 while leaving jumpers JP5, JP7, JP9, JP11, JP13JP15, JP21 and JP36 open. When connecting SPI1 as a slave, ​connecting JP20 enables ​the slave select and serial clock inputs on the [[http://​www.analog.com/​adum3402|ADuM3402]].
  
 These jumper settings are given in the table below: These jumper settings are given in the table below:
  
-|              ^  JP5  ^  JP6  ^  JP7  ^  JP8  ^  JP9  ^  JP10  ^  JP11  ^  JP12  ^  JP13  ^  JP14  ^  JP15  ^  JP16  ^  JP20  ^  JP21  ^ +|              ^  JP5  ^  JP6  ^  JP7  ^  JP8  ^  JP9  ^  JP10  ^  JP11  ^  JP12  ^  JP13  ^  JP14  ^  JP15  ^  JP16  ^  JP20  ^  JP21  ​^ ​ JP36  ^  JP37  ^ 
-^  SPI1 Master ​ |  Connect ​ |  Open  |  Connect ​ |  Open  |  Connect ​ |  Open  |  Connect ​ |  Open  |  Connect ​ |  Open  |  Connect ​ |  Open  |  Open  |  Connect ​/ Floating ​ | +^  SPI1 Master ​ |  Connect ​ |  Open  |  Connect ​ |  Open  |  Connect ​ |  Open  |  Connect ​ |  Open  |  Connect ​ |  Open  |  Connect ​ |  Open  |  Open  |  Connect ​|  Connect ​ |  Open  |  
-^  SPI1 Slave  |  Open  |  Connect ​ |  Open  |  Connect ​ |  Open  |  Connect ​ |  Open  |  Connect ​ |  Open  |  Connect ​ |  Open  |  Connect ​ |  Connect ​ |  Open  |+^  SPI1 Slave  |  Open  |  Connect ​ |  Open  |  Connect ​ |  Open  |  Connect ​ |  Open  |  Connect ​ |  Open  |  Connect ​ |  Open  |  Connect ​ |  Connect ​ |  Open  ​| ​ Open  |  Connect ​ |
  
 \\ \\
Line 23: Line 23:
 {{ :​ezlinx:​isolatedspi2.png?​nolink&​900 |Figure 2. Isolated SPI2 schematic}} {{ :​ezlinx:​isolatedspi2.png?​nolink&​900 |Figure 2. Isolated SPI2 schematic}}
  
-To connect Isolated SPI2 as a master, connect jumpers JP22, JP24, JP26, JP28, JP30 and JP32 while leaving jumpers JP23, JP25, JP27, JP29, JP31 and JP33 open. To connect Isolated SPI2 as a slave, connect jumpers JP23, JP25, JP27, JP29, JP31 and JP33 while leaving jumpers JP22, JP24, JP26, JP28, JP30 and JP32 open. When connecting SPI2 as a slave JP34 should also be connected, enabling the slave select and serial clock inputs on the [[http://​www.analog.com/​adum3402|ADuM3402]].+To connect Isolated SPI2 as a master, connect jumpers JP22, JP24, JP26, JP28, JP30JP32, JP35 and JP38 while leaving jumpers JP23, JP25, JP27, JP29, JP31JP33, JP34 and JP39 open. To connect Isolated SPI2 as a slave, connect jumpers JP23, JP25, JP27, JP29, JP31JP33, JP34 and JP39 while leaving jumpers JP22, JP24, JP26, JP28, JP30JP32, JP35 and JP38 open. When connecting SPI2 as a slave JP34 should also be connected, enabling the slave select and serial clock inputs on the [[http://​www.analog.com/​adum3402|ADuM3402]].
  
  
 These jumper settings are given in the table below: These jumper settings are given in the table below:
  
-|              ^  JP22  ^  JP23  ^  JP24  ^  JP25  ^  JP26  ^  JP27  ^  JP28  ^  JP29  ^  JP30  ^  JP31  ^  JP32  ^  JP33  ^  JP34  ^  JP35  ^ +|              ^  JP22  ^  JP23  ^  JP24  ^  JP25  ^  JP26  ^  JP27  ^  JP28  ^  JP29  ^  JP30  ^  JP31  ^  JP32  ^  JP33  ^  JP34  ^  JP35  ​^ ​ JP38  ^  JP39  ^ 
-^  SPI2 Master ​ |  Connect ​ |  Open  |  Connect ​ |  Open  |  Connect ​ |  Open  |  Connect ​ |  Open  |  Connect ​ |  Open  |  Connect ​ |  Open  |  Open  |  Connect ​/ Floating ​ | +^  SPI2 Master ​ |  Connect ​ |  Open  |  Connect ​ |  Open  |  Connect ​ |  Open  |  Connect ​ |  Open  |  Connect ​ |  Open  |  Connect ​ |  Open  |  Open  |  Connect ​|  Connect ​ |  Open  | 
-^  SPI2 Slave  |  Open  |  Connect ​ |  Open  |  Connect ​ |  Open  |  Connect ​ |  Open  |  Connect ​ |  Open  |  Connect ​ |  Open  |  Connect ​ |  Connect ​ |  Open  |+^  SPI2 Slave  |  Open  |  Connect ​ |  Open  |  Connect ​ |  Open  |  Connect ​ |  Open  |  Connect ​ |  Open  |  Connect ​ |  Open  |  Connect ​ |  Connect ​ |  Open  ​| ​ Open  |  Connect ​ |
  
 \\ \\
resources/eval/ezlinx/isolated-spi.txt · Last modified: 03 Jan 2021 22:04 by Robin Getz