Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:eval:eval-advts4152-ebz [06 Feb 2021 20:56] – [EVAL-ADVTS4152-EBZ Overview] - fix link Robin Getzresources:eval:eval-advts4152-ebz [05 Apr 2021 11:29] (current) Ioana Chelaru
Line 58: Line 58:
  
  
-[[adi> EVAL-ADVTS4152-EBZ]] is consist of three major sections. These are the Fault Protection and Surge Stopper, Step-Down Regulator, Back-Up Supply. These three blocks work together to provide reliable and efficient power to the downstream electronics like VTS. It can operate across a wide range of input voltage of 80V DC and surge voltage of up to 210V.+[[adi>EVAL-ADVTS4152|EVAL-ADVTS4152-EBZ]] is consist of three major sections. These are the Fault Protection and Surge Stopper, Step-Down Regulator, Back-Up Supply. These three blocks work together to provide reliable and efficient power to the downstream electronics like VTS. It can operate across a wide range of input voltage of 80V DC and surge voltage of up to 210V.
  
 EVAL-ADVTS4152-EBZ Block Diagram  EVAL-ADVTS4152-EBZ Block Diagram 
Line 101: Line 101:
 ===== EVAL-ADVTS4152-EBZ Test Set-up Guide========= ===== EVAL-ADVTS4152-EBZ Test Set-up Guide=========
  
-Below set-ups are guide to test the [[adi> EVAL-ADVTS4152-EBZ]].+Below set-ups are guide to test the [[adi>EVAL-ADVTS4152|EVAL-ADVTS4152-EBZ]].
 Follow diagram details and instruction to ensure proper set-up. Follow diagram details and instruction to ensure proper set-up.
  
Line 196: Line 196:
  =====Helpful Links==========  =====Helpful Links==========
  
-  * [[Application Note Page]]+  * Application Note Page
  
 -------------------------------------------------------------------------------------------------------------------- --------------------------------------------------------------------------------------------------------------------
resources/eval/eval-advts4152-ebz.1612641369.txt.gz · Last modified: 06 Feb 2021 20:56 by Robin Getz