This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:eval-advts4152-ebz [06 Feb 2021 20:56] – [EVAL-ADVTS4152-EBZ Overview] - fix link Robin Getz | resources:eval:eval-advts4152-ebz [05 Apr 2021 11:29] (current) – Ioana Chelaru | ||
---|---|---|---|
Line 58: | Line 58: | ||
- | [[adi> EVAL-ADVTS4152-EBZ]] is consist of three major sections. These are the Fault Protection and Surge Stopper, Step-Down Regulator, Back-Up Supply. These three blocks work together to provide reliable and efficient power to the downstream electronics like VTS. It can operate across a wide range of input voltage of 80V DC and surge voltage of up to 210V. | + | [[adi>EVAL-ADVTS4152|EVAL-ADVTS4152-EBZ]] is consist of three major sections. These are the Fault Protection and Surge Stopper, Step-Down Regulator, Back-Up Supply. These three blocks work together to provide reliable and efficient power to the downstream electronics like VTS. It can operate across a wide range of input voltage of 80V DC and surge voltage of up to 210V. |
EVAL-ADVTS4152-EBZ Block Diagram | EVAL-ADVTS4152-EBZ Block Diagram | ||
Line 101: | Line 101: | ||
===== EVAL-ADVTS4152-EBZ Test Set-up Guide========= | ===== EVAL-ADVTS4152-EBZ Test Set-up Guide========= | ||
- | Below set-ups are guide to test the [[adi> EVAL-ADVTS4152-EBZ]]. | + | Below set-ups are guide to test the [[adi>EVAL-ADVTS4152|EVAL-ADVTS4152-EBZ]]. |
Follow diagram details and instruction to ensure proper set-up. | Follow diagram details and instruction to ensure proper set-up. | ||
Line 196: | Line 196: | ||
| | ||
- | * [[Application Note Page]] | + | * Application Note Page |
-------------------------------------------------------------------------------------------------------------------- | -------------------------------------------------------------------------------------------------------------------- |