This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:eval-adum141e1s [02 Aug 2018 14:45] – [Example Test Procedure] Jonathan Harris | resources:eval:eval-adum141e1s [11 Jan 2021 09:02] (current) – Fixed bad link for AN-1478 Ioana Chelaru | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== EVALUATING THE ADUM141E1S QUAD CHANNEL ISOLATOR | ====== EVALUATING THE ADUM141E1S QUAD CHANNEL ISOLATOR | ||
===== Preface ===== | ===== Preface ===== | ||
- | The [[adi> | + | The [[adi>EVAL-ADUM141E1S|EVAL-ADUM141E1S]] supports the ADUM141E1S quad-channel digital isolator based on Analog Devices, Inc., iCoupler® technology. Combining high speed CMOS and monolithic air core transformer technology, the [[adi>ADuM141ES|ADUM141E1S]] provideds outstanding performance characteristics superior to alternatives such as optocoupler devices and other integrated couplers. The [[adi>ADuM141ES|ADUM141E1S]] offers low propagation delay and low pulse width distortion as well a tight channel matching. The [[adi>ADuM141ES|ADUM141E1S]] features two different fail-safe options by which the outputs transition to a pre-determined state when the input power supply is not applied or the inputs are disabled. |
\\ | \\ | ||
\\ | \\ | ||
- | Complete specifications for the [[adi>ADUM141E1S|ADUM141E1S]] are provided in the [[adi>ADUM141E1S|ADUM141E1S]] data sheet available from Analog Devices, Inc., and should be consulted in conjunction with this Wiki user guide when using the evaluation board. | + | Complete specifications for the [[adi>ADuM141ES|ADUM141E1S]] are provided in the [[adi>ADuM141ES|ADUM141E1S]] data sheet available from Analog Devices, Inc., and should be consulted in conjunction with this Wiki user guide when using the evaluation board. |
\\ | \\ | ||
\\ | \\ | ||
===== Overview ===== | ===== Overview ===== | ||
- | The [[adi>ADUM141E1S|EVAL-ADUM141E1S]] board, shown in Figure 1, can be used to evaluate the performance and data sheet specifications of the [[adi>ADUM141E1S|ADUM141E1S]]. Figure 2 shows the schematic of the [[adi>ADUM141E1S|EVAL-ADUM141E1S]] circuit which can be used to test the accuracy of the [[adi>ADUM141E1S|ADUM141E1S]] and perform other tests. The [[adi> | + | The [[adi>ADuM141ES|EVAL-ADUM141E1S]] board, shown in Figure 1, can be used to evaluate the performance and data sheet specifications of the [[adi>ADuM141ES|ADUM141E1S]]. Figure 2 shows the schematic of the [[adi>ADuM141ES|EVAL-ADUM141E1S]] circuit which can be used to test the accuracy of the [[adi>ADuM141ES|ADUM141E1S]] and perform other tests. The [[adi>EVAL-ADUM141E1S|EVAL-ADUM141E1S]] is a 4-layer PC board, complete with ground and power layers as shown in the Evaluation Board Schematics and Artwork section. |
===== Helpful Documents ===== | ===== Helpful Documents ===== | ||
- | * [[adi>ADUM141E1S|ADUM141E1S]] military data sheet | + | * [[adi>ADuM141ES|ADUM141E1S]] military data sheet |
* [[adi> | * [[adi> | ||
- | * [[adi> | + | * [[adi>media/ |
* [[adi> | * [[adi> | ||
* [[adi> | * [[adi> | ||
Line 20: | Line 20: | ||
| | ||
===== Evaluation Board Files ===== | ===== Evaluation Board Files ===== | ||
- | The evaluation board layout, BOM, and schematic files for the [[adi> | + | The evaluation board layout, BOM, and schematic files for the [[adi>EVAL-ADUM141E1S|EVAL-ADUM141E1S]] board can be downloaded from the links below. |
**DISCLAIMER: | **DISCLAIMER: | ||
Line 37: | Line 37: | ||
=====Evaluation Board ===== | =====Evaluation Board ===== | ||
- | {{ : | + | {{ : |
=====Evaluation Board Schematic===== | =====Evaluation Board Schematic===== | ||
- | {{ : | + | {{ : |
- | Figure 2 shows the [[adi>ADUM141E1S|ADUM141E1S]] schematic of the [[adi> | + | Figure 2 shows the [[adi>ADuM141ES|ADUM141E1S]] schematic of the [[adi>EVAL-ADUM141E1S|EVAL-ADUM141E1S]] evaluation board. U1 is the [[adi>ADuM141ES|ADUM141E1S]] in the center of the board and Pin 1 is the top-left pad with respect to the notch in the silkscreen’s package outline. |
====Equipment Required==== | ====Equipment Required==== | ||
Line 54: | Line 54: | ||
====Power Input==== | ====Power Input==== | ||
- | Each side of the [[adi>ADUM141E1S|ADUM141E1S]] requires an off-board power source. The power source must be independent if common-mode voltages are applied across the isolation barrier or damage may occure to the power supply. | + | Each side of the [[adi>ADuM141ES|ADUM141E1S]] requires an off-board power source. The power source must be independent if common-mode voltages are applied across the isolation barrier or damage may occure to the power supply. |
Line 63: | Line 63: | ||
- Install the 50Ω input resistors (R6 and R16). | - Install the 50Ω input resistors (R6 and R16). | ||
- Install the 15 pF load capacitors (C8, C9, C10, and C11). | - Install the 15 pF load capacitors (C8, C9, C10, and C11). | ||
- | - Connect the evaluation board to the test equipment. | + | - Connect the evaluation board to the test equipment. |
- Once the connections have been made in Step 3 (Figure 2) set both output of the power supply to 5V. Enable the outputs. | - Once the connections have been made in Step 3 (Figure 2) set both output of the power supply to 5V. Enable the outputs. | ||
- Configure the pulse generator to produce a 0V – 5V step, 75MHz Square Wave with an offset value of 2.5V. (If using the Agilent B1110A the max amplitude at 75MHz will be 4 V) Enable the pulse generator output. Note: This provides an input to the A Channel (VIA, J1) of the evaluation board. | - Configure the pulse generator to produce a 0V – 5V step, 75MHz Square Wave with an offset value of 2.5V. (If using the Agilent B1110A the max amplitude at 75MHz will be 4 V) Enable the pulse generator output. Note: This provides an input to the A Channel (VIA, J1) of the evaluation board. | ||
- Set the oscilloscope to the following settings: CH1 = 750 mV/div, Time Base = 2 ns/div. | - Set the oscilloscope to the following settings: CH1 = 750 mV/div, Time Base = 2 ns/div. | ||
- Select the following measurements for CH1: Amplitude, Rise Time, Fall Time, and Frequency. | - Select the following measurements for CH1: Amplitude, Rise Time, Fall Time, and Frequency. | ||
- | - Use the N2796A active probe to capture the A Channel Output (VOA) at connector J5 (a 75 MHz square with an amplitude of approximately 5 V should be visible). An example plot is shown below in Figure 3.{{ : | + | - Use the N2796A active probe to capture the A Channel Output (VOA) at connector J5 (a 75 MHz square with an amplitude of approximately 5 V should be visible). An example plot is shown below in Figure 3.{{ : |
- Check the supply current on both outputs of the power supply to ensure that IDD1 and IDD2 does not exceed 25 mA. | - Check the supply current on both outputs of the power supply to ensure that IDD1 and IDD2 does not exceed 25 mA. | ||
- | - Repeat steps 6 and 7 for any of the remaining channels desired for test (B, C and/or D) by connecting the pulse generator to the appropriate input channel and the oscilloscope to its corresponding output. Refer to the table below for connections: | + | - Repeat steps 6 and 7 for any of the remaining channels desired for test (B, C and/or D) by connecting the pulse generator to the appropriate input channel and the oscilloscope to its corresponding output. Refer to the table below for connections: |