This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:eval-adm2795e-ardz [26 Jan 2018 10:36] – Richard Anslow | resources:eval:eval-adm2795e-ardz [26 Jan 2018 10:40] (current) – Richard Anslow | ||
---|---|---|---|
Line 43: | Line 43: | ||
----- | ----- | ||
===== Isolated Motor Control System using Arduino Form Factor Rapid Development Platforms ===== | ===== Isolated Motor Control System using Arduino Form Factor Rapid Development Platforms ===== | ||
+ | \\In this set-up the stimulus from an ultrasonic sensor at one end of the RS-485 bus controls a motor and gearing or fan assembly at the far end of the bus. | ||
+ | The EVAL-ADICUP-360 Arduino form factor compatible ARM Cortex-M3 Development Platform accepts inputs from a standard ultrasonic sensor. | ||
+ | The EVAL-ADICUP-360 outputs are used to control the EVAL-ADM2795EARDZ logic signals. The first EVAL-ADM2795EARDZ then transmits to a second EVAL-ADM2795EARDZ node over 10 meters of RS-485 Category 5e cable. | ||
+ | On the far end of the bus, the second receiving EVAL-ADM2795EARDZ, | ||
{{: | {{: | ||
{{: | {{: | ||
- | \\ In this set-up the stimulus from an ultrasonic sensor at one end of the RS-485 bus controls a motor and gearing or fan assembly at the far end of the bus. | + | |
- | The EVAL-ADICUP-360 Arduino form factor compatible ARM Cortex-M3 Development Platform accepts inputs from a standard ultrasonic sensor. | + | |
- | The EVAL-ADICUP-360 outputs are used to control the EVAL-ADM2795EARDZ logic signals. The first EVAL-ADM2795EARDZ then transmits to a second EVAL-ADM2795EARDZ node over 10 meters of RS-485 Category 5e cable. | + | |
- | On the far end of the bus, the second receiving EVAL-ADM2795EARDZ, | + | |
------ | ------ | ||
Line 74: | Line 74: | ||
*Application Note: http:// | *Application Note: http:// | ||
- | |||
----------- | ----------- |